×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 92022677, Entry date: 08/10/2017
(13)
Rate

SINAMICS G/S: Generating GSDML files for S120, S150, G130, G150, S110

  • Entry
  • Associated product(s)
Generating specific GSDML files for SINAMICS S120, S150, G130, G150, S110 configurations, to integrate this drives at STEP7 (TIA-Portal) with this structure.

Task

At the present time, SINAMICS S120, S150, G130 and G150 devices are not integrated in Startdrive. As a consequence, drives based on these devices are currently configured in STARTER.
TIA Portal applications, which use these SINAMICS devices must use GSD configurations for these devices.


Configuring in parallel in the TIA Portal and in STARTER is possible under the following general conditions:
 

  • Telegrams are configured manually and separately in the TIA Portal and in STARTER.
  • Telegram configurations are not synchronized with one another.
  • Changes to the configuration must be updated on both sides.

As a consequence, configuring costs increase and also the possibility of making mistakes.

Solution
The scripts presented here generate GSDML files for specific drive configurations. The script runs in the context of STARTER. The user installs the generated GSDML files in the TIA Portal, and there they are directly available in the hardware catalog.

The above-mentioned points can be significantly improved with this approach:

  • Telegrams are only configured in STARTER.
  • Configuring telegrams in the TIA Portal is synchronized with configuring telegrams in STARTER.
  • Changes to the configuration only have to be updated in STARTER.

Requirement
Configuring a drive must comply with the following conditions in order that the script can create a GSDML file: 

  • It involves a SINAMICS S120, S150, G130 or G150 device.
  • It involves a SINAMICS S110 device
  • The device has firmware version V4.3 or higher.
  • Cyclic communication is configured via PROFINET; optionally on board or with the Communication Board Extension (CBE).
  • Cyclic communication is realized via the logical IF1 interface.

Note
If you are interested, please contact your local sales partner.
Contact partners worldwide

Downloads

Content of downloads

Application description V2.2
 Registrierung notwendig   Registrierung notwendig  GenerateGsdmlFile_V2_2_0.zip (665,5 KB) 

SHA-512 Checksum:  Registrierung notwendig  SHA512.txt (1 KB)

Information about SHA-512 checksum: 109483101

Additional Search Terms
Scripting, motioncontrol_apc_applications

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.