×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 92022677, Entry date: 08/10/2017
(16)
Rate

SINAMICS G/S: Generating GSDML files for S120, S150, G130, G150, S110

  • Entry
  • Associated product(s)
Generating specific GSDML files for SINAMICS S120, S150, G130, G150, S110 configurations, to integrate this drives at STEP 7 (TIA-Portal) with this structure.

Task
The SINAMICS S120, S150, G130 and G150 inverters can be configured with both Stardrive or STARTER. 


TIA Portal applications that use SINAMICS devices configured with STARTER must rely on GSD configurations of these devices.


Configuring in parallel in the TIA Portal and in STARTER is possible under the following general conditions:

  • Telegrams are configured manually and separately in the TIA Portal and in STARTER.
  • Telegram configurations are not synchronized with one another.
  • Changes to the configuration must be updated on both sides.

As a consequence, configuring costs increase and also the possibility of making mistakes.

Solution
The scripts presented here generate GSDML files for specific drive configurations. The script runs in the context of STARTER. The user installs the generated GSDML files in the TIA Portal, and there they are directly available in the hardware catalog.

The above-mentioned points can be significantly improved with this approach:

  • Telegrams are only configured in STARTER.
  • Configuring telegrams in the TIA Portal is synchronized with configuring telegrams in STARTER.
  • Changes to the configuration only have to be updated in STARTER.

Requirement
Configuring a drive must comply with the following conditions in order that the script can create a GSDML file: 

  • It involves a SINAMICS S120, S150, G130 or G150 device.
  • It involves a SINAMICS S110 device
  • The device has firmware version V4.3 or higher.
  • Cyclic communication is configured via PROFINET; optionally on board or with the Communication Board Extension (CBE).
  • Cyclic communication is realized via the logical IF1 interface.

Note
If you are interested, please contact your local sales partner.
Contact partners worldwide

Downloads

Content of downloads

Application description V2.2

  Generating_GSDML_files_for_SINAMICS_drives_V2_2_EN.pdf (704,5 KB)

Script V2.2.1:

 Registrierung notwendig  GenerateGsdmlFile_V2_2_1.zip (358,3 KB)

SHA-512 Checksum:  Registrierung notwendig  SHA512_V2_2_1.txt (1 KB) 

Information about SHA-512 checksum: 109483101

Additional Search Terms
Scripting, motioncontrol_apc_applications

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.