×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 92045471, Entry date: 11/17/2014
(3)
Rate

SINAMICS S120: OA-Applikation VIBX (Vibration Extinction)

  • Entry
  • Associated product(s)
ask/application: For a stacker crane, mast oscillation is excited when accelerating and braking. The throughput and storage capacity/storage height are restricted as a result of this mast oscillation. Not only this, a reinforced mechanical design is required as a result of this mast oscillation.

Task
For a stacker crane, mast oscillation is excited when accelerating and braking. The throughput and storage capacity/storage height are restricted as a result of this mast oscillation. Not only this, a reinforced mechanical design is required as a result of this mast oscillation.

Solution
The SINAMICS Technology Extension "Vibration extinction" (VIBX, vibration extinction) is an extension for the SERVO and VECTOR drive objects. The Technology Extension for SINAMICS S120, SINAMICS S150 and for SINAMICS Integrated – in versions SIMOTION D4x5-2 and SINUMERIK 840D sl – can be extended from SINAMICS firmware V4.4 and higher.

VIBX significantly reduces mast oscillation when accelerating and decelerating, which means that it is adequately stationary in a verifiable shorter time. As a consequence, a stacker crane can handle more goods in the same time period.

Advantages:

  • Increases the handling capacity.
  • Increases the warehouse capacity/warehouse height.
  • Possibility of reducing construction costs.
  • Energy usage is reduced as a result of the lower weight.
  • Less stress on the material.

A setpoint filter is implemented in the Technology Extension. The objective of the axis setpoint filter to change the setpoint of an axis so that there is as little oscillation as possible excited in the natural frequency range of the moving mechanical components.

Two application modes are supported:

  • Application mode "Basic positioner (EPos) and position control (LR)".
    The setpoint filter acts between the EPos and position controller (LR) function modules. The position setpoint and velocity setpoint are filtered between the output of EPos and the input to the position controller (LR).
  • "Dynamic Servo Control (DSC)" application mode
    The setpoint filter acts between the PROFIdrive receive telegram for DSC and the DSC controller. Process data XERR and NSOLL_B are filtered before they are used in the DSC controller.

The filter characteristics can be set using the frequency and the damping (attenuation).

Via a connector input, in operation, the filter frequency can be linearly changed between two extreme values. This means that the filter frequency can be tracked to follow the changing natural frequency of a mechanical system (e.g. as a result of different load states) (online frequency change). 

   

P1.png

A detailed description of VIBX is provided under the release for delivery 109738131 of VIBX V1.3.

Note
If you are interested, please contact the respective sales person.
Contact persons worldwide

Supplementary search terms
motioncontrol_apc_applications, SINAMICS OA, OA application, VIBX, Vibration Extinction, Regalbediengerät, stacker cranes, rack feeder, 

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit