×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 92346281, Entry date: 04/05/2019
(5)
Rate

PROFIBUS GSD files : ET 200AL

  • Entry
  • Associated product(s)
PROFIBUS GSD files ET 200AL : Station type IM 157-1 DP

DESCRIPTION:

Station type: IM 157-1 DP (Rev.5)
Order no.: 6ES7 157-1AA00-0AB0
Version: V1.4.7 (03/2019))
 Registrierung notwendig  ET200AL_IM157-1DP.zip (62,5 KB)
SHA256 checksum: E72DC19695908ABEADCDCEC3D6A9EA133FDC81EB750549A3826C88654B5FECDC

Station type: IM 157-1 DP (Rev.3)
Order no.: 6ES7 157-1AA00-0AB0
Version: V1.4.7 (03/2019)
 Registrierung notwendig  ET200AL_IM157-1DP_Rev3.ZIP (56,0 KB)
SHA256 checksum: AA33A460150B5B60D750C386313B398CB2979B8493A13B3677731A82B160DF31

FAQ: How do you determine the SHA-256 or SHA-512 checksum of a file?  109483101 


An additional GSD file in revision 3 is now available in addition to the previous PROFIBUS GSD files with revision 5

Using the GSD files

  • This GSD file is only to be used if the configuration cannot be done using the GSD file revision 5.
  • The revision 3 GSD files can be used with all engineering tools that do not support the revision 5 GSD files e.g. COM PROFIBUS. There are also many older engineering tools that do not allow the installation of newer GSD files because they contain newer key words.
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.