×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 92522512, Entry date: 03/13/2018
(7)
Rate

SINAMICS S120 firmware version 4.7 HF32

  • Entry
  • Associated product(s)
You can find the SINAMICS S120 firmware version 4.7 HF32 here.
Description
The version designation on the memory card (CF) is SINAMICS S120 V04.07.00.32
The internal version number of the firmware is SINAMICS S120 V04.74.35.23.

When upgrading, please observe the instructions for the firmware update.


Third-party software – license conditions and copyright notes

You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the file READ_OSS.HTM file.


Special note for resellers

The notes and the license conditions contained in the READ_OSS.HTM file must be passed on to the purchaser in order to avoid the reseller and purchaser from violating the licensing conditions.


Availability of the source code

Some license conditions of third-party software components used in this product may oblige us to provide you with the source text and further information for these components. You can find this information either directly on the product itself or with the product (e.g. on the mass memory, DVD). Should this not be possible due to technical reasons, Siemens will gladly send you this OSS source code; however, you will have to pay the handling costs. Please contact the address specified at the end of this section in this regard:


Siemens AG

Digital Factory

Customer Services DF&PD

DF CS SD CCC TS

Gleiwitzer Strasse 555

90475 Nuremberg, Germany

Internet: http://www.siemens.com/automation/support-request

+49 (911) 895-7222

support.automation@siemens.com


READ_OSS.HTM (1.6 MB)


Secondary conditions for SINAMICS S120
  sinamics_s120_v4_7_restrictions.pdf (43,1 KB) 


Function restrictions for the SINAMICS S120 for the CU320-2 and CU310-2 that have been withdrawn

 Registrierung notwendig  S120_Corrected_Functional_Restrictions_V4_7_HF_32_en.pdf (4,8 KB)


Instructions to update the firmware of the SINAMICS S120 CU320-2 and CU310-2
When upgrading, please observe the instructions for the firmware update:
  instructions_firmware_update_s120.pdf (1,2 MB)


SINAMICS S120 firmware version V4.7 HF32 for the CU320-2 and CU310-2

The following software can be downloaded:

Note
From version V4.7 HF7, the runtime SINAMICS S120 firmware as download is not subject to any export restrictions, as the output frequency has been limited to 550 Hz.
It is not subject to the Iran embargo, and is not listed in the EC Dual Use regulation.
It does not involve a US product.
If higher output frequencies are required, then the "High output frequency" license must be purchased, Article number: 6SL3074-0AA02-0AA0.
It can also be ordered as Z option J01 together with the CF card. (see 104020669)
The license "High output frequency" is subject to export restrictions.

Alternatively, a new memory card (CF) with the following Article number can be used:

  • without performance enhancement:
    Article number: 6SL3054-0EH00-1BA0
  • with performance enhancement firmware option:
    Article number: 6SL3054-0EH01-1BA0


List of faults and alarms

The "alarmlist_*.xml" are not necessary for the correct operation of the firmware and the associated STARTER. They only contain a text-based export of the "Alarm messages" of the S120 in the "xml" format (this format guarantees a correct text-based representation, independent of the wide range of fonts that exist worldwide; this means that they can be converted error-free into other formats).
Customers occasionally request this exported text so that they can use it in their own applications or integrate it into external devices. As a consequence, as far as the S120 product is concerned, no additional support can be guaranteed here.

alarmlist_s_v04703584_deu.xml (3.3 MB)

alarmlist_s_v04703584_eng.xml (3.3 MB)

alarmlist_s_v04703584_esp.xml (3.4 MB)

alarmlist_s_v04703584_fra.xml (3.5 MB)

alarmlist_s_v04703584_ita.xml (3.5 MB)

alarmlist_s_v04703583_chs.xml (3.0 MB)


GSD files for project integration into the PROFIBUS configuring tool
The PROFIBUS GSD files are saved on the SINAMICS S120 CompactFlash card under the following path:
..\SIEMENS\SINAMICS\DATA\CFG
However, they can also be downloaded: (see 49216293)


GSDML files for integrating projects into the PROFINET configuring tool
The PROFINET GSDML files are saved on the SINAMICS S120 CompactFlash card under the following path:
..\SIEMENS\SINAMICS\DATA\CFG
However, they can also be downloaded: (see 49217480)
EDS files for integrating projects into the CANopen configuring tool
see 48351511


STARTER
Within the scope of firmware version V4.7 the new version of STARTER V4.4 will also be made available (see 93904214).
As an alternative to the installation of STARTER V4.4, you can also extend existing STARTER V4.3 SP2 or V4.3 SP3 installations by installing the available drive SSPs (see 26233208) for Firmware V4.7. Thus, you can use the new functions included in the Firmware V4.7 with STARTER.
Startdrive
SINAMICS S120 is not supported in Startdrive V13.
STARTER is used for commissioning.
The hardware configuration of the S120 on the TIA Portal can be implemented using GSD/GSDML files, see73257075 (manual configuring) and92022677 (configuring using STARTER script).
DCC (Drive Control Chart)
see 98206100
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.