×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 92554110, Entry date: 01/30/2019
(13)
Rate

SINAMICS G120 firmware version 4.7 HF11

  • Entry
  • Associated product(s)
In this article you will find the download as well as the ordering information for SINAMICS G120 multicard with version V4.7 HF11.

Important Note

The SINAMICS G120 Firmware Version 4.7 HFx has achieved the milestone P.M400 "Phase-out announcement" on 01.10.2018. With this background, we recommend using the latest SINAMICS G firmware. The milestone P.M410 "Product Cancellation" for V4.7 HFx is planned for 01.10.2019.


For the latest firmware version please refer to the article 67364620.


Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the READ_OSS.HTM file.


Special information for resellers 
The information and the license terms in the READ_OSS.HTM file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.


Availability of Source Code
Certain license conditions of third-party software components used in this product may require Siemens to provide you with the source code and additional information for such components. In most cases, Siemens provides this information on or with the device. In case Siemens is technically unable to do so, you may request a copy of of this OSS source code against payment of shipping and handling charges. Please send your request to the address provided at the end of this section.


Siemens AG 

Digital Factory

Customer Services DF&PD

DF CS SD CCC TS

Gleiwitzer Str. 555

90475 Nuernberg, Deutschland

Internet: http://www.siemens.com/automation/support-request

Tel.: +49 911 895 7222


  READ_OSS.HTM (1,8 MB)


Actual list of secondary conditions for the SINAMICS G120, Firmware Version V4.7

   SINAMICS_G120_V4_7_Restrictions.pdf (38,0 KB)

 

Functional restrictions which have been corrected for the SINAMICS G120 Firmware V4.7 HF11
  Corrected_Functional_Restrictions_G120_V4_7_HF11.pdf (31,9 KB)

 

Instructions for updating the firmware of the SINAMICS G120
When upgrading, please refer to the instructions, Chapter "Firmware update" in the operating instructions of the particular Control Unit.

For example, the instructions for the firmware update for the CU240B-2 and CU240E-2 can be found here:
  Instructions_Firmwareupdate_G120_CU240BE-2_ENG.pdf (389,6 KB) 

Note:
The zip file must be saved unpacked on the SD card in the root directory.
An SD memory card with at least 256 MB must be used.
Memory cards larger than 2 GB are not supported.
The SINAMICS SD-CARD 512 MB empty can be obtained via order number 6SL3054-4AG00-2AA0.

 

Provision of the SINAMICS G120 multicard V4.7 HF11

The content of the SINAMICS G120 multicard described above can be downloaded here:

Content of the SINAMICS G120 multicard V4.7 HF11:
  SINAMICS_G120_firmware_V4_7_HF11.zip (79,0 MB)

Note:

SINAMICS G120 runtime firmware is not currently subject to export restrictions from version V4.7 HF3 and above as the output frequency has been limited to 550 Hz.
It is not subject to the Iran embargo and is not listed in the EC Dual-Use Regulation (AL:N).
It is not a US product (ECCN:N).

Alternatively, the SINAMICS G120 multicard V4.7 (SD-Karte) SD card) can be ordered using the following article number 6SL3054-7EH00-2BA0.

 

List of faults and alarms

List of faults and alarms for CU230P-2
The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120P in the "xml" format.
Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the G120P product is concerned, no additional support can be guaranteed here.

  alarmlist_g120_cu230p_v04702900_chs.xml (365,9 KB)
  alarmlist_g120_cu230p_v04702900_eng.xml (394,9 KB)
  alarmlist_g120_cu230p_v04702900_esp.xml (416,2 KB)
  alarmlist_g120_cu230p_v04702900_fra.xml (426,1 KB)
  alarmlist_g120_cu230p_v04702900_ita.xml (421,6 KB)
  alarmlist_g120_cu230p_v04703500_deu.xml (400,0 KB)

 

List of faults and alarms for the CU240B-2 and CU240E-2
The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120 in the "xml" format.
Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the G120 product is concerned, no additional support can be guaranteed here.

  alarmlist_g120_cu240b_e_v04702900_chs.xml (589,5 KB)
  alarmlist_g120_cu240b_e_v04702900_eng.xml (636,1 KB)
  alarmlist_g120_cu240b_e_v04702900_esp.xml (669,9 KB)
  alarmlist_g120_cu240b_e_v04702900_fra.xml (688,1 KB)
  alarmlist_g120_cu240b_e_v04702900_ita.xml (675,1 KB)
  alarmlist_g120_cu240b_e_v04703500_deu.xml (645,0 KB)

 

List of faults and alarms for the CU240D-2 and CU250D-2
The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120D in the "xml" format.
Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the G120D product is concerned, no additional support can be guaranteed here.

  alarmlist_g120d_v04702900_chs.xml (684,5 KB)
  alarmlist_g120d_v04702900_eng.xml (740,2 KB)
  alarmlist_g120d_v04702900_esp.xml (777,3 KB)
  alarmlist_g120d_v04702900_fra.xml (798,1 KB)
  alarmlist_g120d_v04702900_ita.xml (784,4 KB)
  alarmlist_g120d_v04703500_deu.xml (746,7 KB)

 

List of faults and alarms for CU250S-2 
The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120 in the "xml" format.
Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the G120 product is concerned, no additional support can be guaranteed here.

  alarmlist_g120_cu250s_v04702900_chs.xml (1,1 MB)
  alarmlist_g120_cu250s_v04702900_eng.xml (1,2 MB)
  alarmlist_g120_cu250s_v04702900_esp.xml (1,2 MB)
  alarmlist_g120_cu250s_v04702900_fra.xml (1,3 MB)
  alarmlist_g120_cu250s_v04702900_ita.xml (1,2 MB)
  alarmlist_g120_cu250s_v04703500_deu.xml (1,2 MB)

 

List of faults and alarms of the G120C
The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120C in the "xml" format.
Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the G120C product is concerned, no additional support can be guaranteed here.

  alarmlist_g120c_v04702900_chs.xml (395,6 KB)
  alarmlist_g120c_v04702900_eng.xml (429,7 KB)
  alarmlist_g120c_v04702900_esp.xml (453,8 KB)
  alarmlist_g120c_v04702900_fra.xml (466,0 KB)
  alarmlist_g120c_v04702900_ita.xml (457,7 KB)
  alarmlist_g120c_v04703500_deu.xml (435,3 KB)

 

List of faults and alarms of the G110M
The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120C in the "xml" format.
Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the G110M product is concerned, no additional support can be guaranteed here.

  alarmlist_g110m_v04702900_chs.xml (508,4 KB)
  alarmlist_g110m_v04702900_eng.xml (549,3 KB)
  alarmlist_g110m_v04702900_esp.xml (579,9 KB)
  alarmlist_g110m_v04702900_fra.xml (594,9 KB)
  alarmlist_g110m_v04702900_ita.xml (584,8 KB)
  alarmlist_g110m_v04703500_deu.xml (556,9 KB)

 


GSD files for project integration into the PROFIBUS configuring tool


PROFIBUS GSD files can be downloaded in the following entries:

 

GSDML files for project integration into the PROFINET configuring tool

PROFINET GSDML files can be downloaded in the following entries:

 

EDS files for project integration into the CANopen configuring tool

The EDS files for project integration in the CANopen configuring tools can be downloaded from the following entry:  (see 48351511)

 


STARTER


Within the framework of the Firmware Version V4.7, the new STARTER V4.4 version will also be provided (see 93904214).
As an alternative to the installation of STARTER V4.4, you can also supplement existing STARTER V4.3 SP2 or V4.3 SP3 installations by installing the available drive SSPs (see 26233208) for the Firmware V4.7.
Thus, you can use the functional innovations included in the Firmware V4.7 with STARTER.

 

Startdrive

Within the framework of the Firmware Version V4.7, the Hardware Support Package V4.7 will be provided for Startdrive V13 (see 68034568).
With the import of the Hardware Support Package in an existing Startdrive V13 installation, you can use the functional innovations in firmware V4.7 with Startdrive.
It is not necessary to install a new Startdrive version.

 

IOP

Note:
If the SINAMICS G120P (CU230P-2), G120 (CU240B-2, CU240E-2, CU250S-2), G120D (CU240D-2, CU250D-2), G120C and G110M products are operated with firmware version 4.7 and an Intelligent Operator Panel (IOP) is used, then for this purpose, the IOP firmware from version V1.5 should be used. (see 100427102)