×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 92556243, Entry date: 05/19/2014
(0)
Rate

What is the max. cable length for the SITRANS FX300?

  • Entry
  • Associated product(s)

The max. cable length for the SITRANS FX300 is 15m.

The menu 3.6.1 for setting the cable length allows a max. value of 30m. This is an error in the firmware of the transmitter. The max. cable length for the remote version is specified with 15m. A sensor cable with 30m length is not available. Selecting cable length "30m" can compromise the functionality of meter and may result in errors in flow measurement. 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.