×
Siemens Industry Online Support
Siemens AG
Entry type: Application example, Entry ID: 93148272, Entry date: 09/07/2015
(11)
Rate

Demo project for SIMATIC WinCC V7.3

  • Entry
  • Associated product(s)
This page contains the current SIMATIC WinCC V7.3 demo projects (example configuration) for download. The “use-case oriented” projects provide a guided tour through the plant with different user names.

Description
The demo project is configured in German and English.
The UI language can be set individually in the development environment of SIMATIC WinCC V7.3.
The configured national languages are also available in Runtime.

Demo projects for WinCC V7.3

Documentation for the demo project
  Documentation (1,7 MB)

WinCC Automation Highlights (Videos)
Videos on tips & tricks as well as WinCC V7 functionalities can be found in the entry ID 74509647.

SIMATIC WinCC SCADA in Online Support
The overview page displays all information on the topic of WinCC at a glance.
You can find the page in entry ID: 93906404
.

Demo projects for SIMATIC WinCC V7.2
Demo projects of the previous WinCC V7.2 version can be found in the following entry ID: 76879225.

Demo project for WinCC Runtime Professional V13
Demo project for WinCC Runtime Professional including Multitouch gestures can be found in the following entry ID: 109478972.

SIMATIC WinCC V7.3 Trial Software, Europa and Asia
The software required for using the demo projects can also be obtained as trial software (for 30 days) from the sales partner responsible.
Siemens Contact Person

Trial DVD WinCC V7.3
Article No: 6ZB5370-1DN70-2FA7

Further information on WinCC V7.3 is available in the following entry ID: 97493192

WinCC V7.3 supports the following Microsoft operating systems
For WinCC single-user projects and client projects

  • Windows 8.1 (Professional / Enterprise, 32-bit)

  • Windows 8.1 (Professional / Enterprise, 64-bit)

  • Windows 7 SP1 (Ultimate / Professional / Enterprise, 32-bit)

  • Windows 7 SP1 (Ultimate / Professional / Enterprise, 64-bit)

  • Windows Server 2012 R2 (Standard 64-bit)

  • Windows Server 2008 R2 SP1 (Standard 64-bit)

  • Windows Server 2008 SP2 (Standard 32-bit)

For WinCC Server

  • Windows 8.1 (Professional / Enterprise 64-bit)

  • Windows Server 2012 R2 (Standard 64-bit)

  • Windows Server 2008 R2 SP1 (Standard 64-bit)

  • Windows Server 2008 SP2 (Standard 32-bit)

Last Changes
First publication


Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.
Support to the statistics
With this function the IDs found are listed according to number (format .txt).

Generate list
Copy URL
mySupport Cockpit
Related links