×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 93839056, Entry date: 02/19/2020
(22)
Rate

SIMATIC STEP7 Reaktionszeit Tabelle / Safety Reaction Time Table SIMATIC S7-1500F / S7-1200F

  • Entry
  • Associated product(s)
SIMATIC STEP7 Reaktionszeit Tabelle / Safety Reaction Time Table SIMATIC S7-1500F / S7-1200F

  

Description 


The S7 Reaction Time Table (S7Safety_RTTplus*.xls) is used for theoretical estimation of F-execution times, F-runtimes, F- monitoring times and F-response times in connection with the SIMATIC S7-1500F and SIMATIC S7-1200FC CPUs during system layout.


The execution times of the F-application blocks, the F-FBD/F-LAD elements and the runtime of the F-runtime group were determined based on SIMATIC STEP7 Safety Advanced.


Provision must still be made for measurement of the actual values in the real system, taking into account all actuators and sensors and any constraints. The S7Safety_RTTplus*.xls is not legally binding and must not replace system acceptance testing or be incorporated into the system documentation.


The runtime times are valid under the following conditions:


The "Max. runtime of F-runtime group" can be extended due to, among other things, the communication load (e.g. S7 communication, PROFINET IO communication, PG/OP communication), the processing of higher-priority interrupts and the testing and commissioning functions.
 You can determine the effect of these factors based on the documentation and configuration of the standard system and add it to the value calculated up to now. The application is documented in the manual "SIMATIC Industrial Software SIMATIC Safety - Configuration and Programming" Appendix A "Monitoring and response times". 54110126

 

For statements about the expected reaction time  when integrating a SIMATIC Mobile Panel, please refer to article  27097159 "How do you incorporate the execution times of the F blocks for the Mobile Panel ... ".

 

 

 Registrierung notwendig  s7safety_rttplus.xlsm (563,3 KB)

 

The language switch is located within the table (Row 1, Column K: German/English/French)


When using Office365 applications, note that the corresponding macros have to be activated separately.


Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.