×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 94770057, Entry date: 08/05/2014
(0)
Rate

SIMOTION: Download during RUN

  • Entry
  • Associated product(s)

Summary
The FAQ describes the system interrelationships and the necessary settings so that a download can be executed while a SIMOTION SCOUT V4.4 project is running on a SIMOTION CPU.

Question
What has to be taken into account so that a download is successful during RUN?

Answer
With a download, SIMOTION SCOUT checks all modified sources, so that consistent data is always loaded.

From SIMOTION SCOUT V4.4 and higher, selected, individual sources can be loaded (consistent subsets).
This is true for a download at STOP as well as a download during RUN.
Therefore, only transparent and understandable changes should be made for a download during RUN.

 See attached PDF file:

 FAQ-02YFY319-DLimRUN_en.pdf ( 630 KB )