×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 95848378, Entry date: 05/02/2017
(5)
Rate

Which modules of the Siemens portfolio support PROFIenergy functions?

  • Entry
  • Associated product(s)
In production sites, breaks occur consistently. With PROFIenergy you can turn off specific consumers that are not needed during the break and in this way significantly reduce energy costs.

The matrix provided in this entry includes the following information:

  • Which modules support PROFIenergy?
  • Which PROFIenergy functions are supported by the modules?
  • In which programming environment can the modules be used?
  • What are the other requirements for using the modules with PROFIenergy?

Download
The download includes the Excel file "Matrix-PROFIenergy.xlsx".
Copy the "Matrix-PROFIenergy.xlsx" file into a separate directory and then open the file with a double-click.

 Registrierung notwendig  Matrix-PROFIenergy.xlsx (5,5 MB)

Additional Information
Detailed information on the topic of the PROFIenergy is available in the sample application in Entry ID 96837137 and elsewhere.

Additional Keywords
ET 200S, ET 200SP, ET 200AL, Motor starter, SENTRON PAC, 3VA2 ETUs, Comfort Panel, SINAMICS, ET 200pro FC2, SIMATIC, IPC, SIMOCODE, Soft starter, S7-300, S7-400, S7-1500, SINUMERIK, SIMOTION, PC CPs, SITOP PSU8600

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit