×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 95854032, Entry date: 07/10/2014
(0)
Rate

Why does the CP 1616 / CP 1604 as PROFINET IO controller and/or PROFINET IO device not go into data exchange mode after the configuration has been successfully loaded?

  • Entry
  • Associated product(s)

Description
The CP 1616 and the CP 1604 can be used as PROFINET IO controller and/or PROFINET IO device. For this function it is not sufficient just to load the configuration into the CP 1616 or CP 1604. The PROFINET IO function needs an application based on the IO Base of the PROFINET IO programming interface.

Further Information

  • Detailed information about the IO Base user programming interface is available in the programming manual in Entry ID 26435491.
  • The procedure of an IO Base controller user program in the IO controller is given in section 3.3.
  • The procedure of an IO Base device user program in the IO device is given in section 6.3.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.