×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 96839331, Entry date: 09/29/2017
(12)
Rate

Process automation with the SIMATIC PCS 7 CPU 410-5H controller

  • Entry
  • Associated product(s)
The main focus of this document is to describe scenarios which explain relevant functions of the CPU 410-5H Process Automation in the AS 410 and illustrate advantages over the complementary S7-400 systems.

Contents
The CPU 410-5H is a controller specially designed for process automation which is versatile in use. With robust, high performance hardware, it covers the entire performance spectrum of the AS 412 to AS 417 complementary systems.


In this document, scenarios are described which explain relevant functions of the CPU 410-5H Process Automation in the AS 410 and illustrate advantages over the complementary S7-400 systems. Additionally you will gain an overview of important configuration steps and hints.
You will find information on the following topics in the document:
  • General information on the CPUs of the AS410
  • Advantages of the CPU 410-H
  • Configuring the communications interface and establishing the connection between the ES and the AS
  • Type Change in RUN (TCiR) function and Configuration in Run (CiR/H-CiR)
  • Configuration of the PN/Ethernet interfaces
  • Upgrade with CPU 410 Expansion Packs (Process objects and PN Red License)

Applicability

  • CPU 410-5H Process Automation
  • From SIMATIC PCS 7 V8.1

Documentation for PCS 7 V9.0
  Process automation with the SIMATIC PCS 7 CPU 410-5H controller – PCS 7 V9.0 (2,9 MB)

Documentation for PCS 7 V8.2
  Process automation with the SIMATIC PCS 7 CPU 410-5H controller – PCS 7 V8.2 (1,9 MB)

Documentation for PCS 7 V8.1
  Process automation with the SIMATIC PCS 7 CPU 410-5H controller – PCS 7 V8.1 (1,9 MB)

Product and ordering information
SIMATIC PCS 7 CPU 410-5H Process Automation - Product and ordering information

Video
SIMATIC PCS 7 CPU 410-5H - A Process Controller for Everything
YouTube

Further information
You can find an overview of all of the relevant information for implementing PROFINET solutions in SIMATIC PCS 7 in the following entry: 72887082

Last changes

Notes added