×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 98161300, Entry date: 08/27/2021
(167)
Rate

SIMATIC Automation Tool - the commissioning and service operation tool for SIMATIC modules

  • Entry
  • Associated product(s)
Here you can deploy the SIMATIC Automation Tool as a Trial Download.

After a control program is created and verified with the Siemens TIA Portal software, the SIMATIC Automation Tool can be used in the field for operating and maintaining SIMATIC S7-1200, S7-1500, ET 200, HMI, SITOP, SCALANCE switches, RFID and MOBY Ident modules.

Automation Tool operations:

  • Scan a PROFINET/Ethernet network and identify all devices connected to the network
  • Flash device LEDs or HMI screens to physically locate a device
  • Create a table that maps the accessible devices on the network
  • Assign addresses (IP, subnet, gateway) and station name (PROFINET device)
  • Set the time in a CPU to the current time in your PG/PC
  • Download a program to a CPU and HMI panels
  • Put a CPU in RUN or STOP mode
  • Perform a CPU Memory reset

  • Backup/Restore CPU or HMI data to/from a backup file
  • Upload service data from a CPU
  • Upload of service data from ET200 devices
  • Read the diagnostics buffer from a CPU
  • Reset a CPU to factory default settings
  • Update firmware in a CPU and attached modules
  • Ability to load firmware update files on devices and activate the new firmware later
  • Support for CPUs connected through a CM (Communications Module) or CP (Communications Processor)
  • Upload, download, or delete Recipe data (stored at SMC) from a CPU
  • Upload or delete Data log data (stored at SMC) from a CPU
  • Information in Device table for CPUs: TIA Portal version and configured CPU version
  • Document and save your network information
    • In a standard text .csv file or
    • An encrypted & password protected .sat file
  • Use the API to create custom .NET applications based on the functionality available in the SIMATIC Automation Tool
  • Advanced features:
    • Up to 10 concurrent connections.
    • Scheduler for scheduling device operations on a time and frequency of your choosing
    • Card browser for working with files and folders on SIMATIC memory cards in your CPUs
    • Archiving capabilities for SAT projects and associated file data
    • Ability to insert multiple devices in one operation
    • Support for devices behind a NAT router


Operations can be performed in parallel to multiple devices at one time.

As a registered customer, you can download the trial version for SIMATIC Automation Tool and test it for 21 days.
To ensure continued support of the complete feature set after the trial period expires, you can order one of these software options from Online Software Delivery: 

 ProductArticle number  

SIMATIC Automation Tool V4
Basic Feature Set

 6ES7853-1AE04-0YA5 Online Software Delivery (OSD)Download with Floating License

SIMATIC Automation Tool Advanced V4

 6ES7853-1AE14-0YA5
SIMATIC Automation Tool Advanced V4;
Powerpack V3/V4 -> Advanced V4
 6ES7853-1KE04-0YA5

SIMATIC Automation Tool V3

 6ES7853-1AE03-0YA5

When updating the SIMATIC Automation Tool version, always update to the latest version available. The previous versions are only intended as backup to allow a downgrade to the original version. This is not known to have been necessary.

SIMATIC Automation Tool Support Model

Siemens provides bug and security fixes only for the latest released software version. This means that Siemens only monitors the latest software version for security vulnerabilities. Siemens does not monitor “Backup only” software for security vulnerabilities.

Download

The software is subject to export restrictions; the download is only available to registered users. Please bear in mind that because of strong demand, the registration for export-restricted downloads can take several days. see also: 109744535 


 VersionSetup files Manual 
 V04.00.03

Recommended for update:

 Download unterliegt Exportcontrolle  SIMATIC_Automation_Tool_V4_0_SP3.exe (433,8 MB)

SHA-256 checksum 1)

 Download unterliegt Exportcontrolle  SIMATIC_Automation_Tool_V4_0_SP3.txt (1 KB)

Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party
software contained in this product, particularly open source
software, as well as applicable licensing terms of such
third-party software in the SAT.ReadMe.OSS.V4.0_SP3_en-US file. 

Special information for resellers
The information and the license terms in the

SAT.ReadMe.OSS.V4.0_SP3_en-US file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendig  SAT.ReadMe.OSS.V4.0.SP3.en-US.pdf (1,1 MB)

User guide Edition V4.0 SP3, 09/2021:

SAT.UserGuide.V4.0.SP3.en-US_en-US.pdf

Product Information V4.0 SP3, 09/2021:

SAT.ProductInformation.V4.0.SP3.en-US_en-US.pdf

Installation Notes V4.0 SP3, 09/2021:

SAT.InstallationNotes.V4.0.SP3.en-US_en-US.pdf

Device catalog with specification of the supported modules and their functional scope:

 Registrierung notwendig  SAT_DeviceCatalog_V4.0_SP3.xlsx (1,1 MB)

  V04.00.02

Backup only:

 Download unterliegt Exportcontrolle  SIMATIC_Automation_Tool_V4_0_SP2.exe (397,0 MB)

SHA-256 checksum 1)

 Registrierung notwendig  SIMATIC_Automation_Tool_V4_0_SP2.txt (1 KB) 

Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party
software contained in this product, particularly open source
software, as well as applicable licensing terms of such
third-party software in the SAT.ReadMe.OSS.V4.0_SP2_en_US file. 

Special information for resellers
The information and the license terms in the

SAT.ReadMe.OSS.V4.0_SP2_en_US file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendig  SAT.ReadMe.OSS.V4.0_SP2_en_US.pdf (2,9 MB)

User guide Edition V4.0 SP2, 03/2021:

SAT.UserGuide.V4.0.SP2.en-US.pdf

Product Information V4.0 SP2, 03/2021:

SAT.ProductInformation.V4.0.SP2.en-US.pdf

Installation Notes V4.0 SP2, 03/2021:

SAT.InstallationNotes.V4.0.SP2.en-US.pdf

Device catalog with specification of the supported modules and their functional scope:

 Registrierung notwendig  SAT_Device_Catalog_V4.0_SP2.xlsx (808,7 KB)

  V04.00.01

Backup only:

 Download unterliegt Exportcontrolle  SIMATIC_Automation_Tool_V4_0_SP1.exe (397,0 MB)

SHA-256 checksum 1)

 Registrierung notwendig  SIMATIC_Automation_Tool_V4_0_SP1.txt (1 KB)

Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party
software contained in this product, particularly open source
software, as well as applicable licensing terms of such
third-party software in the SAT.ReadMe.OSS.V4.0_SP1_en_US file. 

Special information for resellers
The information and the license terms in the

SAT.ReadMe.OSS.V4.0_SP1_en_US file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendig  SAT.ReadMe.OSS.V4.0_SP1_en_US.rtf (3,2 MB)

User guide Edition V4.0 SP1, 11/2020:

SAT.UserGuide.V4.0.SP1.en-US.pdf

Product Information V4.0 SP1, 11/2020:

SAT.ProductInformation.V4.0.SP1.en-US.pdf

Installation Notes V4.0 SP1, 11/2020:

SAT.InstallationNotes.V4.0.SP1.en-EN.pdf

Device catalog with specification of the supported modules and their functional scope:

 Registrierung notwendig  SAT_Device_Catalog.xlsx (809,4 KB)

 V04.00.00

Backup only:

 Download unterliegt Exportcontrolle  SIMATIC_Automation_Tool_V4_0.exe (397,0 MB)

SHA-256 checksum 1)

 Registrierung notwendig  SIMATIC_Automation_Tool_V4_0.txt (1 KB)

Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party
software contained in this product, particularly open source
software, as well as applicable licensing terms of such
third-party software in the SAT.ReadMe.OSS.V4.0.en-US file. 

 Registrierung notwendig  SAT.ReadMe.OSS.V4.0.en-US.rtf (2,0 MB)

Special information for resellers
The information and the license terms in the

SAT.ReadMe.OSS.V4.0.en-US file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

User guide Edition V4.0, 07/2020:

 Registrierung notwendig  SAT.UserGuide.V4.0.en-US.pdf (4,4 MB)

Product Information V4.0, 07/2020:

 Registrierung notwendig  SAT.ProductInformation.V4.0.en-US.pdf (208,5 KB)

Installation Notes V4.0, 07/2020:

 Registrierung notwendig  SAT.InstallationNotes.V4.0.en-US.pdf (368,4 KB) 

Device catalog with specification of the supported modules and their functional scope

 Registrierung notwendig  Device_Catalog_V1_1R_SAT.xlsx (806,2 KB)

 V03.01.04

Backup only:

  Download unterliegt Exportcontrolle  SIMATIC_Automation_Tool_V3_1_SP4.exe (386,9 MB) 

SHA-256 checksum 1):

 Registrierung notwendig  SIMATIC_Automation_Tool_V3_1_SP4.txt (1 KB)

Third-party software - Licensing terms and copyright
information

You can find the copyright information for third-party
software contained in this product, particularly open source
software, as well as applicable licensing terms of such
third-party software in the SAT.ReadMe.OSS.V3.1.SP4.en-US file.


Special information for resellers
The information and the license terms in the
SAT.ReadMe.OSS.V3.1.SP4.en-US file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendig  SAT.ReadMe.OSS.V3.1.SP4.en-US.rtf (6,3 MB)

User guide Edition V3.1 SP4, 12/2019:

 Registrierung notwendig  SAT.UserGuide.V3.1.SP4.en-US.pdf (4,5 MB)

Product Information V3.1 SP4, 12/2019:

 Registrierung notwendig  SAT.ProductInformation.V3.1.SP4.en-US.pdf (214,3 KB)


Installation Notes V3.1 SP4, 012/2019:

 Registrierung notwendig  SAT.InstallationNotes.V3.1.SP4.en-US.pdf (356,6 KB)

 V03.01.03

Backup only:

 Download unterliegt Exportcontrolle  SIMATIC_Automation_Tool_V3_1_SP3.exe (353,0 MB) 

SHA-256 checksum 1):

 Registrierung notwendig  SIMATIC_Automation_Tool_V3_1_SP3.txt (1 KB)

Third-party software - Licensing terms and copyright
information

You can find the copyright information for third-party
software contained in this product, particularly open source
software, as well as applicable licensing terms of such
third-party software in the SAT.ReadMe.OSS.V3.1.SP3.en-US file.


Special information for resellers
The information and the license terms in the
SAT.ReadMe.OSS.V3.1.SP3.en-US file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendig  SAT.ReadMe.OSS.V3.1.SP3.en-US.rtf (4,3 MB)

User guide Edition V3.1 SP3, 04/2019:

SAT.UserGuide.V3.1.SP3.en-US_en-US.pdf

Product Information V3.1 SP3, 04/2019:

SAT.ProductInformation.V3.1.SP3.en-US_en-US.pdf

Installation Notes V3.1 SP3, 04/2019:
SAT.InstallationNotes.V3.1.SP3.en-US_en-US.pdf

 V03.01.02


removed


User guide Edition V3.1 SP2, 11/2018:

SAT.UserGuide.V3.1.SP2.en-US.pdf

Product Information

SAT.ProductInformation.V3.1.SP2.en-US.pdf

Installation Notes

SAT.InstallationNotes.V3.1.SP2.en-US.pdf

  V03.01.01

removed


User guide Edition V3.1 SP1, 05/2018:

  simatic_automationtooluserguide_v3_1_sp1_en-US.pdf (5,6 MB)

Product Information

simatic_automationtoolproductinfo_v3_1_sp1_en-EN.pdf

Installation Notes

simatic_automationtoolinstallationnotes_v3_1_sp1_ en-EN.pdf

 V03.01.00

removed


User guide Edition V3.1, 10/2017:

simatic_automationtooluserguide_V3_1_201710_en-US.pdf

V03.00.00

removed


User guide Edition V3.0, 06/2017:  AutomationToolUserGuide_V3_0_201706_en-US_en-US.pdf 

  SIMATICAutomationToolReleaseNotes_V3_0_201706_en-US.pdf (247,2 KB)

V02.01.01

removed

   AutomationToolUserGuide_V2_1_1_201610_en-US.pdf (2,3 MB) 
V02.01.00

removed

   AutomationToolReleaseNotes_V2_1_201607_en-US.pdf (256,8 KB) 

  AutomationToolUserGuide_V2_1_201607_en-US.pdf (2,3 MB)

V02.00.00

removed

   AutomationToolReleaseNotes_V2_201509_en.pdf (236,0 KB)

  AutomationToolUserGuide_V2_201509_en.pdf (2,1 MB)

V01.00.02

removed

 
V01.00.01

removed

 

 1) Information on SHA-256 109483101 


 Update V04.00.03

Update version V04.00.03 (V4.0 SP3)  replaces version V04.00.02 and includes the following new features:

  • Secure communication to CPUs using certificates and TLS
  • Configuration data protection
  • PROFIsafe address assignment for local and distributed F-IO
  • Creation of memory cards
  • Support for additional reset to factory defaults options
  • Support for additional options when formatting a memory card
  • Support for S7-1500 R/H CPUs
  • Changes in licensing requirements for features
  • Support for devices and firmware versions that TIA Portal V17 supports
  • Some usability improvements such as:
    • Enhancements for inserting single or multiple devices into the Device table
    • Filtered scan
    • Event log filtering
    • Reminder for activating downloaded firmware in two-step firmware updates


 Update V04.00.02

Update version V04.00.02 (V4.0 SP2)  replaces version V04.00.01 and includes the following new features:

  • Support for additional operations for devices and versions as included in the Device Catalog
  • Two-step firmware update for additional SITOP power supplies
  • Improved file and folder handling in the Card Browser - Simplification for distribution of mutliple files
  • Ability to insert multiple devices behind NAT routers into the Device table from Microsoft Excel files - enhanced handling for associated Router IP addresses


 Update V04.00.01

Update version V04.00.01 (V4.0 SP1)  replaces version V04.00.00 and includes the following new features:

  • Support for SIMATIC HMI Unified Comfort Panels 
  • Support for SIMATIC Drive Controller CPU 1504D TF and CPU 1507D TF
  • Support for SIFLOW FCT070


 Update V04.00.00

Update version V04.00.00  replaces version V03.01.04 (V3.1 SP4) and includes the following new features:

  • Changes in product licensing: Basic, Advanced, and 21-day trial
  • Support for CPUs connected through a CM (Communications Module) or CP (Communications Processor)
  • Ability to load firmware update files on devices and activate the new firmware later
  • User interface enhancements
  • Upload of service data from ET200 devices
  • Additional information in Device table for CPUs: TIA Portal version and configured CPU version
  • Additional module support: 
    • 6ES7 136-6AB00-0CA1 ET200SP, F-AI 4xU 0..10V HF
    • 6ES7 137-6EA00-0BA0 ET 200SP CM CAN
  • Advanced features (need an Advanced license for use: 6ES7853-1AE14-0YA5):
    • Scheduler for scheduling device operations on a time and frequency of your choosing
    • Card browser for working with files and folders on SIMATIC memory cards in your CPUs
    • Archiving capabilities for SAT projects and associated file data
    • Ability to insert multiple devices in one operation
    • Support for devices behind a NAT router


 Update V03.01.0

Update version V03.01.04 (V3.1 SP4) replaces version V03.01.03 and includes the following new features:

  • Support new firmware (TIA Portal V16related) for existing devices as listed in the device catalog 
  • Support HMI devices with customer specific veneers
  • Support new product families, basic DCP functions plus FW update (if applicable and as specified in the device catalog)
    • Support TIM 1531 IRC
    • Support SIMATIC PN/J1939 LINK
    • Support Micro drives PDC 50 F and F-IO
    • Support SIRIUS Soft Starter 3RW5 PN 
    • Support RFID Reader devices 
    • Support SINAMICS devices S210 
    • Support SIMATIC PN/M-Bus LINK 
    • Support SIMATIC ITC V3 (SIMATIC Industrial Thin Client) 


 Update V03.01.03

Update version V03.01.03 (V3.1 SP3) replaces version V03.01.02 and includes the following new features:

  • Free 21-day trial license
  • Support for additional devices and versions as listed in the device catalog  
  • Export of device diagnostics
  • Export of PC data
  • Enhanced export of device information
  • Ability to back up and restore HMI recipes and HMI user administration data
  • Partial support for S7‑300 and S7‑400 devices, as identified in the Device Catalog
  • Ability to restore Device table column defaults
  • Troubleshooting help for Event Log messages


 Update V03.01.02

Update version V03.01.02 (V3.1 SP2) replaces version V03.01.01and includes the following new features:

  • Support for additional devices and versions as listed in the device catalog. Device families include:
    • Buerkert ET200P pneumatic modules (firmware update only)
    • ET200 eco PN F devices
    • HMI Comfort Pro Panels
    • S7-1500 Software Controllers
    • PN/PN coupler
    • SIMOCODE Pro devices
    • SIRIUS ACT 3SU1 PN devices
  • Updated appearance of the device table that is more similar to the TIA Portal
  • Ability to select a device in the device table and show all references to it
  • Faster method for copying and pasting into multiple device table cells in a column
  • Send a DCP Reset Communication Parameters to devices
  • Improved network scanning to retain previous data until the scan reads the new data
  • Support for Ethernet transfer channel for HMIs
  • Addition of Chinese Simplified language for the SIMATIC Automation Tool user interface and documentation


 Update V03.01.01

Update version V03.01.01 (V3.1 SP1) replaces version V03.01.00:

  • Ability to view the device catalog in Microsoft Excel format, launched from the Help menu
  • Support for additional device families as defined in the device catalog, including the
    following:
    • SCALANCE Industrial Ethernet Switches
    • CPU 1518-4 PN/DP MFP (Multi-Funktional Platform) and CPU 1518-4 PN/DP ODK (Open Development Kit)
    • SIMATIC PN/CAN LinkSupport for new firmware versions of devices, e.g. S7-1500 CPU Firmware V2.5
  • Ability to perform an HMI image update independently of a program update
  • Ability to collect service data that users can send to Siemens in the event of an unexpected
    problem
  • Automated install capability - Silent Mode Installation


 Update V03.01.00

Update version V03.01.00 replaces version V03.00.00:

  • Support for the following operations to Fail-Safe CPUs
    • Program update
    • Restore from backup
    • Reset to factory defaults
    • Format memory
  • Format SIMATIC Memory Card
  • Expanded API
  • Enhanced editing capabilities in the device table


 Update V03.00.00

Update version V03.00.00 replaces version V02.01.01:

  • support additional product families
    • S7-1500T
    • ET 200pro CPU - CPU 1516pro
    • Basic, Comfort, and Mobile HMI’s
    • SITOP power supplies
    • SIMATIC RFID and MOBY Ident modules
  • Supports recipes and data logs
  • Supports 64 bit Windows Operation systems, Windows 7 & Windows 10
  • Supports five languages (German, English, French, Spanish, Italian)
  • Requires a license for unlimited device support - without license key no API support and no mass operation+

Notice: It is recommended to install the SIMATIC Automation Tool V3.0 together with other SIMATIC Software on one PC only if you have the latest SIMATIC software installed for example TIA Portal V14 SP1.


     Update V02.01.01

    Update version V02.01.01 replaces version V02.01.00 and improves the behaviour:

    • support program download based on S7-1200 firmware version V4.2
    • support program download based on S7-1500 firmware version V2.0 
    • firmware update ET200ECO PN, 6ES7141-6BF00-0AB0  
    • 6GK7 542-1AX00-0XE0 CM 1542-1 update firmware correctly
    • program download with password - projects with changed firmware versions


     Update V02.01.00

    Update version V02.01.00 replaces version V02.00.00 and improves the behaviour:

    • by installation setup, if newer TIA Portal versions are installed at the same PC 
    • disabling Reset to Factory operation at S7-1500 based CPU's  


    Update V02.00.00  

    New Features:

    • Support S7-1500 Compact/FailSafe* CPUs incl. central modules and backup/restore
    • Support S7-1200 Failsafe* CPUs incl. central modules
    • Support ET200SP Standard/Failsafe* CPUs incl. central modules and backup/restore
    • Support firmware update of decentralized IO devices – PROFINET and PROFIBUS
    • Improve application & communication performance and usability
      • Skin the application to look like TIA Portal
      • Query the Siemens Support Site (SIOS) for all available FW versions
      • Column filter to more clearness by setting operstions to modules with same characteristic

    *) no support backup/restore, Reset-to-factory and program download for failsafe application

     

    Update V01.00.02  


    V1.0.2 corrects a setup issue  where newer versions of SIMATIC Device Drivers would cause the installation to fail.  This problem is now resolved in the setup.


    Security information:

    Siemens provides products and solutions with industrial security functions that support the secure operation of plants, solutions, machines, equipment and/or networks. They are important components in a holistic industrial security concept.  With this in mind, Siemens’ products and solutions undergo continuous development. Siemens recommends strongly that you regularly check for product updates.
    For the secure operation of Siemens products and solutions, it is necessary to take suitable preventive action (e.g. cell protection concept) and integrate each component into a holistic, state-of-the-art industrial security concept.  Third-party products that may be in use should also be considered.  For more information about industrial security, visit http://www.siemens.com/industrialsecurity.
    To stay informed about product updates as they occur, sign up for a product-specific newsletter.  For more information, visit http://support.automation.siemens.com.

    Security information
    In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
    https://www.siemens.com/cybersecurity#Ouraspiration.
    Rate entry
    no rating
    Requests and feedback
    What do you want to do?
    Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.
    Support to the statistics
    With this function the IDs found are listed according to number (format .txt).

    Generate list
    Copy URL
    Display page in new design
    mySupport Cockpit