×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 98278916, Entry date: 06/19/2015
(0)
Rate

How can I resolve an "SFC" type conflict in projects with protected blocks in TIA Portal V13?

  • Entry
  • Associated product(s)
When the ident application blocks can`t be compile anymore after upgrading a project from TIA Portal V12 to TIA Portal V13, then use the solution which is shown in this entry.

After upgrading a project from STEP 7 Professional V12 (TIA Portal V12) to STEP 7 Professional V13 (TIA Portal V13), ident application blocks (see article ID 109476945), which used to be compilable in TIA Portal V12, now trigger an error message when being compiled in TIA Portal V13.
 


Figure 01

Solution

  1. Open a protected block.
     
  2. When the password prompt appears, click on "Cancel".
     

    Figure 02
     
  3. Open the instructions tab on the right side.
       
  4. Look for the SFC (system and standard function block) which triggered the error message in the basic or extended instructions.
     
  5. In the column "Version", choose the version of the block that is needed to compile the block.


Figure 03

Source of pictures
The pictures in this FAQ were taken from TIA Portal V13.

Safety Guidelines
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions only form one element of such a concept.
Customer is responsible to prevent unauthorized access to its plants, systems, machines and networks. Systems, machines and components should only be connected to the enterprise network or the internet if and to the extent necessary and with appropriate security measures (e.g. use of firewalls and network segmentation) in place.
Additionally, Siemens’ guidance on appropriate security measures should be taken into account. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.
Siemens’ products and solutions undergo continuous development to make them more secure. Siemens strongly recommends to apply product updates as soon as available and to always use the latest product versions. Use of product versions that are no longer supported, and failure to apply latest updates may increase customer’s exposure to cyber threats.
To stay informed about product updates, subscribe to the Siemens Industrial Security RSS Feed under
http://www.siemens.com/industrialsecurity.

Additional Keywords
WRREC, Typkonflikt, MOVE_BLK, Ident Libary, Ident Bibliothek, FB45 TIA

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.