×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 98754979, Entry date: 06/28/2018
(0)
Rate

Firmware Update for S7-1500 TM COUNT 2x24V

  • Entry
  • Associated product(s)
Firmware Update for S7-1500 TM COUNT 2x24V

Description:
When updating the firmware, always update to the latest version available for the product and its respective article number.
The previous versions of the firmware are only intended as backup to allow a downgrade to the original version.

How to update the firmware is described in detail in entry ID 78648446.


Please note the applicable licensing conditions for the module described in the entry SIMATIC S7-1500, ET 200MP, ET 200SP License conditions for technology and communication modules

Overview of article numbers and firmware versions of the S7-1500 TM COUNT 2x24V:

Article number

Software version

Update with...
6ES7550-1AA00-0AB0  
  V1.3.0

Recommended for update:
For a description, see below Update V1.3.0


For STEP 7 as of Version 5.5
 Registrierung notwendig  Classic_6ES7550-1AA00-0AB0_V130.ZIP (296,4 KB)
SHA-256 checksum (Information of SHA-256)
 Registrierung notwendig  Classic_6ES7550-1AA00-0AB0_V130.txt (1 KB) 

For STEP 7 TIA Portal
 Registrierung notwendig  TIA_6ES7550-1AA00-0AB0_V130.ZIP (296,3 KB)
SHA-256 checksum (Information of SHA-256)
 Registrierung notwendig  TIA_6ES7550-1AA00-0AB0_V130.txt (1 KB)

 

V1.1.27

Backup only:
For a description, see below Update V1.1.27

For STEP 7 as of Version 5.5
Classic_5501AA00_V1127.EXE ( 427 KB )

For STEP 7 TIA-Portal
TIA_5501AA00_V1127.EXE ( 428 KB )

 

V1.0.0

Backup only:

For STEP 7 as of Version 5.5
Classic_5501AA00_V100.EXE ( 421 KB )

For STEP 7 TIA-Portal
TIA_5501AA00_V100.EXE ( 421 KB )


Update V1.3.0

New functionality:

  • Support of the "Measuring input" functionality (TO Measuring Input) in "Position detection for "Motion Control" technology object" operating mode.
  • More flexibility when setting the comparison values
  • The "Frequency" parameter can now also be set for the DI function "Capture" to once or periodically. 


Update V1.1.27

The following new function has been implemented:

Firmware version V1.1.27 enables a distributed configuration of the module with PROFIBUS DP and configuration by means of GSD. Due to technical restrictions not all module parameters are available in the GSD. The complete module parameters can be set in the user program via the data record 128. Details are described in the device manual TM Count 2x24V, at entry ID 59193105 


Please note: The last digit of the version number ist due to technical reasons and will not necessarily be incremented without gaps.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.