×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 98957840, Entry date: 07/28/2014
(13)
Rate

Wizard for creating connection data for open TCP/IP communication (Open Communication Wizard).

  • Entry
  • Associated product(s)

Description  
All new SIMATIC S7-CPUs contain an integrated PROFINET interface which in addition to PROFINET also enables TCP/IP communication. The configuration of the TCP/IP communication via this integrated Ethernet interface is is made by using the blocks for open communication. For easy configuration of this open communication (TCP native, ISO on TCP, UDP) we offer you here the Open Communication Wizard (OC Wizard) as a free download.

For open TCP/IP communication via the PROFINET interface of the S7-CPUs, the communication blocks FB65 "TCON", FB66 "TDISCON", FB63 "TSEND" and FB64 "TRCV" are used. For the open communication the parameters for each connection have to be specified in a data block. Using the OC Wizard tool enables simple and clear specification of the connection parameters. Only the parameters necessary for the respective connection type have to be specified via the OC Wizard. The tool then exports a UDT or a DB with all parameters of the connection description into your STEP 7 project. Existing connections can be read, altered, copied and documented. The OC Wizard is automatically integrated into the menu of the SIMATIC Manager. Hence, the OC Wizard can be called directly from the SIMATIC Manager.

Start screen of the OC Wizard

Example project
Using the finished data block we then give a simple example of how the communication is realized in the S7-300 and S7-400 CPU from a program technology point of view using the above blocks. This example shows the configuration and programming of a communication relationship between a CPU319 and a CPU416 via the integrated Ethernet interface and the ISO-on-TCP protocol.

Hardware setup of the example project

Note  
From STEP 7 V5.5 SP1 onward the OC Wizard is also included on the STEP 7 DVD. Here you can download the most current version of the OC Wizard free of charge.

Downloads

Content of Downloads

Download

Documentation
Generating the Connection Data for the open TCP/IP Communication using the Open Communication Wizard.
( 1109 KB )
Code 
Tool "Open Communication Wizard" V2.3.3
( 854 KB )
Project 
STEP 7 V5.5 SP 1 example project
Note
Please change the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" used in this example project, with the current communication blocks from the library "Standard Library" for your own project. You will find the mentioned blocks in the SIMATIC Manager under  "File > Open > Open Project > Libraries > Standard Library > Communication Blocks".
( 277 KB )

Further Information

Title

Link

"System software for S7-300/400 system- and standard functions" manual Entry ID:
1214574
FAQs and further examples for open communication via Industrial Ethernet Entry ID:
29737976
Entry ID:
29737950
Entry ID:
29738463

Security information
Siemens provides products and solutions with industrial security functions that support the secure operation of plants, solutions, machines, equipment and/or networks. They are important components in a holistic industrial security concept. With this in mind, Siemens’ products and solutions undergo continuous development. Siemens recommends strongly that you regularly check for product updates.
For the secure operation of Siemens products and solutions, it is necessary to take suitable preventive action (e.g. cell protection concept) and integrate each component into a holistic, state-of-the-art industrial security concept. Third-party products that may be in use should also be considered. For more information about industrial security, visit
http://www.siemens.com/industrialsecurity.
To stay informed about product updates as they occur, sign up for a product-specific newsletter. For more information, visit
http://support.automation.siemens.com.

Last Changes
Add-on with CPU314, CPU 412

Additional Keywords
PN CPU, 319PN, 314PN, 315PN, 317PN, 412PN, 414PN, 416PN

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.