×
Siemens Industry Online Support
Siemens AG
Entry type: Product note, Entry ID: 98958257, Entry date: 08/01/2014
(4)
Rate

STEP 7 Professional 2010 Service Release 4

  • Entry
  • Associated product(s)

The product DVD of STEP 7 Professional 2010 Service Release 4 (SR4) has been updated with the Service Pack 4 (SP4) of STEP 7 V5.5 plus the latest options of PLCSIM, S7-Graph and S7-SCL, and is now available. The SP4 for STEP 7 V5.5 can also be downloaded free of charge from the Internet (entry ID: 93842624).
Customers with a current Software Update Service agreement ( SUS) for STEP 7 Professional COMBO will receive STEP 7 Professional 2010 SR4 automatically.

Customers without a current SUS agreement for STEP 7 Professional can purchase a Trial License with STEP 7 Professional 2010 SR4 under the order no. 6ES7810-5CC11-0YA7. Alternatively you can also install the Service Packs of the individual products. For example, you can install the SP4 for STEP 7 V5.5 via DVD or Download on STEP 7 Professional 2010 (see entry ID 93842624 ).

Requirements for the installation ofSTEP 7 Professional 2010 SR4:

  • STEP 7 Professional 2010 (with or without Service Release)

Supported operating systems:

  • MS Windows XP Professional  SP2 or SP3
  • MS Windows Server 2003 R2 SP2 standard edition as workstation
  • MS Windows 7 32 Bit Ultimate, Professional and Enterprise (Standard installation), 
    with or without SP. However, the Windows XP mode under Windows 7 is not released
  • MS Windows 7 64 Bit Ultimate, Professional and Enterprise with or without SP
  • MS Windows Server 2008 R2 64 Bit, with or without SP
     

Important:

  • The operating system cannot be changed with the STEP 7 Professional software installed. Before you switch the operating system, please be sure to uninstall STEP 7 Professional and any installed STEP 7 option packages.
  • If you wish to change to Windows 7 64 Bit with STEP 7 Professional, you require the DVD with STEP 7 Professional 2010 SR1 or higher.
  • More information is also available from the file:

Windows 64 Bit Support

The SR4 of STEP 7 Professional 2010 now includes the following updates of the components:

  • STEP 7 V5.5 incl. SP4
  • S7-PLCSIM V5.4 incl. SP5 incl. Hotfix 2
  • S7-SCL V5.3  incl. SP6 incl. Hotfix 2
  • S7-GRAPH V5.3 incl. SP7

Packaging ofSTEP 7 Professional COMBO 

When you order a Floating License of STEP 7 Professional, the DVD with the latest version of STEP 7 Professional V13 will additionally be included with the order. A Combo License Key will be included for this purpose, enabling the parallel operation of STEP 7 Professional 2010 and STEP 7 Professional V13 on one computer.

Trial License 

STEP 7 Professional is also available in the form of a cost-effective Trial License for validation purposes (not for productive use). This DVD enables you to test all software packages on the DVD for 14 days (from the first startup of the software). Thereafter you can purchase a Floating License for STEP 7 Professional to enable the complete software without any additional installation for an unlimited period; alternatively you can purchase the relevant individual Floating License(s) of the above individual components.

Ordering information for theSTEP 7 Professional 2010 SR4 Trial License:

Article Number

Product Name

6ES7810-5CC11-0YA7 SIMATIC STEP7 PROFESSIONAL 2010 SERVICE RELEASE 4
DATA CARRIER INCL. TRIAL LICENSE

 

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.