×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 99086336, Entry date: 09/08/2014
(1)
Rate

How do you configure for a Technology CPU a global measuring probe that is connected to the SINAMICS S120?

  • Entry
  • Associated product(s)

Description
With a global measuring probe you can capture the position of any axis or encoder at the time of measuring.
On the other hand, a local measuring probe can only capture the position of the axis or encoder to whose drive/system it is connected.
The CU310, CU310-2, CU320 and CU320-2 of a SINAMICS S120 have digital inputs/outputs which you can use as global measuring probe inputs.

Instructions
Follow the instructions for configuring a global measuring probe in this document:

T-CPU_global_probe_S120_en.pdf ( 583 KB )

Security notes
Siemens offers products and solutions with industrial security functions which support the secure operation of plants, solutions, machines, devices and/or networks. They are important components in a comprehensive industrial security concept. The Siemens products and solutions continue to be developed under this aspect. Siemens recommends that you keep yourself regularly informed about product updates.
For the safe operation of Siemens products and solutions it is necessary to take appropriate security measures (cell protection concept, for example) and to integrate each component in an overall industrial security concept which is state of the art. This should also cover the third-party products used. Additional information about industrial security is available at:
http://www.siemens.com/industrialsecurity.
In order to keep yourself informed about product updates, we recommend subscribing to our product-specific newsletter. Additional information about this is available at
http://support.automation.siemens.com.

Additional Keywords
T-CPU probe technology

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit