×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 99412263, Entry date: 10/08/2019
(6)
Rate

How do you configure and enable the trace of WinCC V6/V7 and WinCC Professional OPC Servers?

  • Entry
  • Associated product(s)
WinCC V6/V7 and WinCC Professional, with their OPC servers for DA, HDA. A&E and UA provide the option of communication both with Siemens products and with products of third-party manufacturers.

Description
In this context, if problems occur with the function or the configured OPC connection does not behave as expected, you can usually make a trace recording of the OPC communication between WinCC OPC Server and the OPC clients used.
The following instructions are for a recommended way of parameterizing the trace of the OPC servers.

Instructions
Usually all the data of the trace output is required for diagnostics. You can increase the data acquisition period by changing the number and size of the files.
These instructions are for a recommended way of configuring the trace settings when a recording of the OPC communication is required.

Storage locations of the trace configuration and trace files
You enable and configure the OPC server traces depending on the version of WinCC V6/V7 or WinCC Professional you are using. In addition, with OPC you have to differentiate between classic servers and UA servers. We describe the different procedures in the following document.

Documentation
  Documentation (366,8 KB)




Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.