×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 99681025, Entry date: 10/21/2014
(0)
Rate

Setting up a secure VPN Connection between SCALANCE S and CP x43-1 Adv. Using a static IP Address.

  • Entry
  • Associated product(s)
Task Due to increased networking through Ethernet, remote diagnostics and/or remote maintenance are of great importance in modern automation systems. Today's Internet access mechanisms (wireless, broadband) and the security components from Siemens are an ideal combination for industrial remote co...

Task
Due to increased networking through Ethernet, remote diagnostics and/or remote maintenance are of great importance in modern automation systems. Today's Internet access mechanisms (wireless, broadband) and the security components from Siemens are an ideal combination for industrial remote communication.
A VPN tunnel is the typical way to establish a secure connection between two networks (e.g., automation networks or individual devices).
A VPN is a virtual, logical private network based on a publicly accessible infrastructure. Only communication partners that belong to this private network can communicate with each other and exchange information and data. 

This application shows the user how to establish a secure connection between two networks over the Internet with the aid of Siemens' Security Products portfolio.

Solution
The security modules SCALANCE S and CP x43-1 Advanced are used to implement the task.

Hardware configuration

Characteristics
The solution described in this application has the following characteristics:

  • VPN tunnel for flexible access to the automation cell - possible, for example, for a service employee.
  • Controlled, encrypted data traffic between SCALANCE S and CP x43-1 Advanced.
  • High degree of security for machines and plants through the implementation of the cell protection concept.
  • Integrated network diagnostics via SNMP or Syslog.
  • Easy integration into existing networks and protection of devices that do not have their own security functions.
  • Protection of the SIMATIC controller without an additional security module
Downloads
Content of Downloads

Download

Configuration Description 
Setting up a secure VPN Connection between SCALANCE S and CP x43-1 Adv. Using a static IP Address
99681025_CPx43_S6xx_StatischeIP_DOKU_V10_en.pdf ( 2067 KB )

Further Information

Title

Link

Topics Overview: Getting Started with Industrial Remote Communication Entry ID:
64721753
Topics Overview: All-round protection with Industrial Security Entry ID:
50203404



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.