×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 99684399, Entry date: 07/17/2020
(10)
Rate

SINAMICS G/S: PROFINET Connection with LabVIEW

  • Entry
  • Associated product(s)
A SINAMICS converter with PROFINET interface should be connected to a PC with the software LabVIEW from National Instruments.


A SINAMICS converter with PROFINET interface is to be connected to a PC with the software LabVIEW from National Instruments.

Cyclic and acyclic I/O communication shall be realized via any network interface of the used PC. LabVIEW shall operate as PROFINET controller.

Solution
The application example shows how to connect a SINAMICS S120 converter to a standard PC by using a DLL which is integrated and running in LabVIEW. For simpler handling the application example VIs are provided for standard telegrams. Their interface emulates 1:1 the SINAMICS telegram interface:

·         Standard telegram 1 (Closed-loop speed control)

·         Standard telegram 111 (Basic positioner operation)

·         Free telegram configuration

For acyclic communication an example VI is provided to read/write parameters which can be extended when required.



Licensing
The DLL to be tied into LabVIEW is based on the product “PROFINET driver for controllers”.
A runtime license is required (e.g. single license  6ES7195-3AA05-0XA0).

Downloads
  Documentation (1,8 MB) 
 Registrierung notwendig  LabView Library (1,4 MB)
 Registrierung notwendig  Starter Project (507,8 KB) 
 Registrierung notwendig  TIA Portal Project V15.1 (221,1 KB)

Additional Keywords
motioncontrol_apc_applications

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.