×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 99742545, Entry date: 09/11/2014
(1)
Rate

Sample program FM 350-2 zXX34_01_FM350-2.zip for TIA Portal V 11.0 + SP 2

  • Entry
  • Associated product(s)

Description
This sample program, contained in the project zXX34_01_FM350-2, consists of the sample project for the TIA Portal included in the configuration software for the counter module FM 350-2 (see Entry ID 28554065).

Software requirements
STEP 7 Professional (TIA Portal) V11.0 + SP 2 and higher

Structure of the sample program
In this example we operate one FM 350-2 in an S7-300 CPU 315-2 DP in the TIA Portal. The example shows how to use all the functions available for the FM 350-2 from the Technology Instructions.

Installation of the sample program
After downloading the project you must unpack the ZIP archive; a local path in the Engineering Station must be used as target path for the project. After unpacking, start the TIA Portal and open the project in the Portal View. The example described is now available in the Project View.

zXX34_01_FM350-2.zip

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.