×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 99862277, Entry date: 08/15/2014
(140)
Rate

Download of Service Pack 4 for STEP 7 V5.5 Chinese

  • Entry
  • Associated product(s)

DESCRIPTION:

Download of Service Pack 4 (SP4) for STEP 7 V5.5 Chinese

Installation requirements for Service Pack 4:

  • STEP 7 V5.5 Chinese and higher

Please also read the information (What’s NEW, special hints, etc.) which we have compiled for you at entry ID76722700

If you wish to change to a new operating system, please bear in mind the following:

  • The precondition to be able to change the operating system with STEP7 is the Product DVD; for ordering please see entry ID 99861638
  • Before you change the operating system, the License Key must be saved from the PC to a floppy disk or USB stick..  
  • Please also note the changed PC hardware requirements of STEP 7; detailled information is provided in the Readme.rtf of STEP 7.

Download of Service Pack 4 for STEP 7 V5.5 Chinese
 SIMATIC_STEP7_V55_SP4_Chinese.exe (1454003 KB) ( 1454003 KB )

This free download includes the SP4 for STEP 7 V5.5 Chinese and NCM and can only be installed, if STEP 7 V5.5 Chinese has already been installed on the PC.

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.