×
Siemens Industry Online Support
Siemens AG
  • Content
  • Search
  • Index
  • Continuous Function Chart Getting Started
    • Preface
    • Summary
    (1)
    Rate

    Entry type: Manual, Entry ID: 103141768, Entry date: 09/30/2014

    SIMATIC Process Control System PCS 7 Continuous Function Chart Getting Started

    Document: SIMATIC Process Control System PCS 7 Continuous Function Chart Getting Started (04/2014, English)
    Type of topic: Fact

    Preface

    Introduction

    The "Getting Started" documentation provides quick instructions for first-time users to acquaint them with the CFC program package. An tutorial is divided into several tasks and guides you step-by-step from the simples configuration work to the creation of a chart with chart I/Os and the generation of the block in the CFC.


    Note

    You can find a completed example in the SIMATIC Manager with the menu command File > Open... in the "Example Projects" tab under the file name ZDt04_01_CFC (German).
    (English: ZEn..., French: ZFr..., Spanish: ZEs..., Italian: ZIt...)



    This example assumes that the CFC is used in the STEP 7 environment. The STEP 7 basis package, SCL and CFC must be installed. The target system is S7-300 or S7-400.

    You create the "CFCBSP_2" example project described in the following with the SIMATIC Manager.