×
Siemens Industry Online Support
Siemens AG
  • Content
  • Search
  • Index
  • WinCC Professional V13.0
    • Visualize processes
      • Working with system functions and Runtime scripting
        • Runtime behavior in Runtime
          • Executing user-defined functions in Runtime
          • Executing a function list in Runtime
          • Execution of functions and local scripts in Runtime
          • Processing sequence for user-defined functions and system functions
          • Making object properties dynamic in Runtime
    (20)
    Rate

    Entry type: Manual, Entry ID: 92323076, Entry date: 05/13/2014

    WinCC Professional V13.0

    Document: WinCC Professional V13.0 (02/2014, English)
    Type of topic: Fact

    Executing user-defined functions in Runtime

    Principle

    Only one user-defined function at a time is executed in Runtime. If several user-defined functions are waiting to be executed, they are lined up in a queue and executed one after the other.


    Note

    A loop in a user-defined function therefore blocks the execution of the other functions in the queue even if the functions were initiated asynchronously.



    WinCC supports a maximum nesting depth of eight user-defined functions. Note that the nesting depth is not checked.


    Note

    If a user-defined function is configured for the "Runtime stop" event, the only system functions that may be used in this user-defined function are those which are available at the "Runtime stop" event.

    Ensure that the ending of the Runtime is not interfered with by the execution of the user-defined function.




    Note

    Configuration of user-defined functions

    During configuration make sure that not too many user-defined functions are activated at the same time. Avoid a continuous system load of 100%.

    User-defined functions are processed at a lower priority so as not to interfere with the display of values and operability. If system utilization is extreme, the user-defined functions to be executed are therefore first only reserved for execution. The maximum size of the reservation list is dependent on the HMI device and is limited by the maximum permitted number of user-defined functions. For additional information, see the performance features. If more user-defined functions are activated at one time than can be reserved, excess calls are discarded and a system alarm displayed.



    HMI device changeover

    If you use system functions in a customized function which are not available on the set HMI device, you get a warning. In addition, the corresponding system function in the user-defined function will be underlined with a wavy blue line.

    See also

    internal link User-defined functions