×
Siemens Industry Online Support
Siemens AG
  • Content
  • Search
  • Index
  • SIMIT Simulation Framework (SF) with PCS 7 - Getting Started (V8.0)
    • Preface
    (2)
    Rate

    Entry type: Manual, Entry ID: 93763208, Entry date: 06/02/2014

    SIMIT Simulation Framework (SF) with PCS 7 - Getting Started (V8.0)

    Document: SIMIT Simulation Framework (SF) with PCS 7 - Getting Started (V8.0) (05/2014, English)
    Type of topic: Fact

    Preface

    Information about the SIMIT Simulation Framework (SF) with PCS 7 Getting Started

    This Getting Started describes the basic procedures and the interaction of the SIMIT SF software components based on the "color_gs" project.

    Additional information is available in the online help on SIMIT and CTE (Component Type Editor).

    Conventions


    Note

    In this documentation, the names of elements in the software interface are specified in the language of this documentation. If you have installed a multi-language package for the operating system, some of the designations will be displayed in the base language of the operating system after a language switch and will, therefore, differ from the designations used in the documentation.



    In SIMIT SF, you can use standard Windows functions in many situations:

    • Multiple selection using the "CTRL" and "Shift" keys
    • Column sorting in tables by clicking on the column header
    • Use of "drag-and-drop" instead of "copy and paste"

    The individual tutorials in the Getting Started build on one another. For this reason, you should work through all the tutorials in the specified sequence.

    Purpose of this Getting Started documentation

    This document aims to guide you quickly and successfully through the basics of SIMIT SF in interaction with PCS 7. You will get to know many elementary configuration steps and develop an understanding for how SIMIT SF works.

    Requirements for the Getting Started

    The "color_gs" project can be executed on any PC on which the following software is installed:

    • Windows 7 Professional or Ultimate SP1, 32-bit or 64-bit operating system
    • SIMIT V8.0 in product version PROFESSIONAL or ULTIMATE
    • SIMATIC PCS 7, V8.0 or later
    • S7-PLCSIM V5.4 SP5
    • Necessary license keys for the software listed above

    Options for accessing documentation on SIMIT SF

    You can find the complete SIMIT documentation at the following locations:

    • On the SIMIT V8.0 DVD
    • on the Internet
    • The product documentation is installed with the relevant product

    Note

    The statements in the SIMIT readme take precedence over all other SIMIT SF documentation.