Storage concept for external storage media and interfaces for memory cards with HMI Unified Comfort Panel
-
Entry
-
Associated product(s)
Description
When using external storage media with SIMATIC HMI Unified Panels (Basic and Comfort), it is important to ensure the compatibility of the storage devices and correct handling in order to avoid data loss or damage.
Note on HMI Unified Basic Panel
HMI Unified Basic Panels do not have an SD card interface, but only the corresponding USB interface(s). For this reason, the following information on SD card compatibility only applies to the HMI Unified Comfort Panel.
Compatible memory cards
SD cards with 128 GB (NTFS system), for example, are also suitable for Unified Comfort Panels.
There is no clear limit to the storage capacity of the SD card or USB stick. SIMATIC SD memory cards and SIMATIC HMI USB sticks with various storage capacities are approved and guaranteed, including
Product details - SD memory card 6AV6881-0AP40-0AA0 (32 GB)
Product details - SD memory card 6AV6881-0AQ10-0AA0 (2 GB) - (Only suitable as data memory card)
Product details - SD memory card 6AV6881-0AQ40-0AA0 (32 GB)
USB flash drive:
Product details - USB flash drive 6AV6881-0AS42-0AA1 (32 GB)
Further details on HMI panels are available here:
SD memory cards, 512 MB, 2 GB to 32 GB for SIMATIC HMI Panels, HMI Unified and IPC
Notes
- SD memory media with a capacity of 32 GB can be used as system cards for SIMATIC HMI Unified Panels.
- It is also possible to use SD cards with a capacity of more than 32 GB for automatic backup with Unified Comfort Panels. The SD card slot, for example, with models MTP1500, MTP1900 and MTP2200 supports the memory cards SD, SDHC and SDXC. Further details are available in the manual: Unified Comfort Panels - MTP1500, MTP1900, MTP2200 Unified Comfort.
- The FAT32 and NTFS file systems are supported for formatting the data memory card.
- A memory card that has already been used as a system memory card can only be used as a data memory card if it has been formatted beforehand.
Storage types
The SIMATIC HMI Unified Comfort Panels offer a variety of storage types that can be used for storing data and backing up information. The various storage types and their functions and uses are briefly explained in the following.
- Internal memory
The operating system, project files, user administration, parameter sets and other data such as documents or media files are stored in the internal memory. For archives with high read/write cycles, it is preferable to use the memory card instead of the USB interface.
Note
Using the internal memory ensures fast access times and reliable data processing. - Data memory card
Archives, data backups, user data, parameter sets and data for reporting can be stored on the data memory card. When the device is switched off, the consistency of the stored data is only guaranteed with the SIMATIC SD Memory Card of 32 GB or more. It is recommended to regularly back up the data on the data memory card in order to avoid data loss. - System memory card
The system memory card is used to automatically save all data from the operating device's internal memory. It is not visible and cannot be used as a data memory device. The system memory card is inserted into the slot provided and is secured by a safety slide.
At the links below you will find technical data and information on the compatibility of SD memory cards with SIMATIC HMI Unified Comfort Panels:
- German
- Spanish
Entry belongs to product tree folder(s):
- Automation Technology Operator control and monitoring systems Operator devices Advanced HMI Panel-based SIMATIC HMI Unified Comfort Panels SIMATIC HMI Unified Comfort Panels Standard
- Automation Technology Operator control and monitoring systems Operator devices Advanced HMI Panel-based SIMATIC HMI Unified Comfort Panels SIMATIC HMI Unified Comfort Panels PRO
- Automation Technology Operator control and monitoring systems Operator devices Basic HMI Unified Basic Panels
- You want to discuss in our forum and exchange experiences with other users
- You have a technical question / problem: Ask the Technical Support
- You want to create CAx data for one or more products
- You would like to send us feedback on this Entry