- Save filter
- Load filter
- e-mail on update
This entry gives you information about importing EPLAN Electric P8 macros in the edz format in EPLAN
What changes to product markings and technical documentation resulted from the update of the standard IEC 60947-4-1: Low-voltage switchgear and controlgear - Part 4-1: Contactors and motor starters - Electromechanical contactors and motor starters with current status Edition 4.0 of 2018?
This article contains information on how operating voltage, operating current, motor current setting and short-circuit breaking capacity must be reduced in relation to the installation height (sea level).
This entry contains a list of the B10 values / failure rates of electromechanical SIRIUS and SENTRON products
This entry provides information on the diagnostic coverage level.
This article contains information on the dynamic behavior of various types of contactors.
This entry contains information about Fuseless Load Feeders with rated operational voltage of 230V AC
This FAQ describe how to order the Product Catalog CA01 on DVD.
This FAQ describe what is to consider when replacing an older motor with efficiency classes (eff3, eff2, eff1, or IE1, IE2) with a high-efficiency motor of efficiency class IE3.
QUESTION: Who is responsible for issuing certificates of origin and certificates of conformity (EN 10204-2004-2-1), test reports and factory certificates for products from Amberg (LZA)? ...
QUESTION: What Safety Integrity Level SIL is achievable with SIRIUS subsystems or subs ...
QUESTION: Can SILCL 1 in compliance with IEC 62061 be achieved with a subsystem consis ...
QUESTION: ISO 13849-1 – Application Explanations How are the PFHD values in the i...
QUESTION: Why may “non-electrotechnical components”, e.g. valves, also be calculated on the basis of IEC 62061? ...
QUESTION: Is it allowed to switch only 2 phases of a 3-phase load? ...
QUESTION: How must switching devices be protected against overload and short-circui ...
QUESTION: What pulling forces apply for round copper conductors that are connected to ...
QUESTION: What are the consequences if the short-circuit protection of auxiliary co ...
QUESTION: What is the behaviour of Low-Voltage switchgear under conditions of very ...
QUESTION: What is the maximum permissible temperature on the plastic surface and connections of Low-Voltage Switchgear? ...