3RT2926-1BC00-ZX90
SIRIUS NG CONTACTORS ACCESSORY
SURGE SUPPRESSOR, VARISTOR, AC 48...127V, DC 70...150V, FOR MOTOR CONTACTORS SZ S0, MULTI-UNIT PACKAGING

  • Save filter
  • Load filter
  • email on update
32
Entries
Filtered by
'
3RT2926-1BC00-ZX90
'
 
Entries per page: 20 50 100
...
1
2
...
FAQ Diagnostic coverage level to be specified and achievable safety integrity level for subsystems or SRP/CS with electromechanical components

This entry provides information on the diagnostic coverage level.

09/28/2018
ID: 35444114
(4)
FAQ What is the difference between positively driven contact elements of contactor relays and mirror contacts of power contactors?

This article contains a statement on the difference between the terms mirror contact and positively driven contact.

09/21/2018
ID: 109758261
(1)
FAQ What safety level can be reached when combining a contactor with a circuit-breaker for fail-safe switching?

This entry contains information about what safety level can be reached when combining a contactor with a circuit-breaker

07/16/2018
ID: 40349715
(5)
FAQ General: Import of EPLAN Electric P8 macros at edz-Format

This entry contains information about import EPLAN Electric P8 macros at edz-Format in EPLAN

12/04/2017
ID: 48074331
(7)
FAQ General: How to order the Product Catalog CA01

This FAQ describe how to order the Product Catalog CA01 on DVD.

07/20/2015
ID: 21656919
(3)
FAQ What must be taken into account for industrial controls when replacing a motor with an IE3 motor in an existing system?

This FAQ describe what is to consider when replacing an older motor with efficiency classes (eff3, eff2, eff1, or IE1, IE2) with a high-efficiency motor of efficiency class IE3.

06/16/2015
ID: 109477525
(3)
FAQ General mounting position of +/-45° during max. 10 minutes for 3RT2 and 3RH2

03/27/2015
ID: 108914982
(0)
FAQ Certificates of origin, certificates of conformity, test reports, factory certificates for products from the distribution center in Amberg (Lieferzentrum Amberg (LZA)).

QUESTION: Who is responsible for issuing certificates of origin and certificates of conformity (EN 10204-2004-2-1), test reports and factory certificates for products from Amberg (LZA)? ...

01/26/2015
ID: 99684616
(3)
Product note Delivery release: Addition of size S2 contactors to the SIRIUS modular system

SIRIUS Innovations size S2 is the further development of the SIRIUS modular system up to 37kW with its wide portfolio of switching, protection and monitoring devices, load feeders, and function modules. ...

10/20/2014
ID: 103599229
(1)
08/06/2014
ID: 35444144
(0)
FAQ Achievable SIL with SIRIUS subsystems or subsystem elements that have a low demand rate according to IEC 61511

QUESTION: What Safety Integrity Level SIL is achievable with SIRIUS subsystems or subs ...

08/06/2014
ID: 35444323
(1)
FAQ PFHD values in the informative annex K, Table K.1 of the ISO 13849-1 standard

QUESTION: ISO 13849-1 – Application Explanations How are the PFHD values in the i...

08/05/2014
ID: 35444036
(0)
FAQ Calculation of “non-electrotechnical components” permissible on the basis of IEC 62061

QUESTION: Why may “non-electrotechnical components”, e.g. valves, also be calculated on the basis of IEC 62061? ...

05/27/2014
ID: 35444396
(0)
FAQ General: Is it mandatory to switch all phases of a 3-phase load?

QUESTION: Is it allowed to switch only 2 phases of a 3-phase load? ...

05/20/2014
ID: 21656588
(0)
FAQ Regulation for protecting switching devices against overload and short-circuits

QUESTION: How must switching devices be protected against overload and short-circui ...

05/19/2014
ID: 91198957
(0)
FAQ Pulling forces for conductors with Cage Clamp connection technology

QUESTION: What pulling forces apply for round copper conductors that are connected to ...

05/13/2014
ID: 21656695
(1)
FAQ Surface treatment of the 3RT19, 3RT29, 3RA27, 3RA28 and 3RA29 front-mounted function module's plug-connectors

QUESTION: What is the surface treatment of the 3RT19, 3RT29, 3RA27, 3RA28 and 3RA29 ...

05/08/2014
ID: 21653834
(0)
FAQ Fuses and miniature circuit breakers for the short-circuit protection of auxiliary contacts

QUESTION: What are the consequences if the short-circuit protection of auxiliary co ...

05/08/2014
ID: 21656724
(0)
FAQ Behaviour of Low-Voltage switchgear under conditions of very low air pressure or vacuum

QUESTION: What is the behaviour of Low-Voltage switchgear under conditions of very ...

04/04/2014
ID: 21656902
(1)
FAQ 3RT19/3RT29 Accessories and Spare Parts: Acceptance test of a surge suppressor (varistor)

QUESTION: How is the procedure to do an acceptance test for a surge suppressor (varistor)? ANSWER:...

09/02/2013
ID: 55644481
(0)
 
Entries per page: 20 50 100
...
1
2
...