×
Siemens Industry Online Support
Siemens AG
Filter criteria for entries
All Products My Products
Product tree
 
 
Clear all filters
Product
Search product
Entry type
 
Date

3SE5232-0HC03-8AA5
SIRIUS POSITION SWITCH
SIRIUS POSITION SWITCH PLASTIC HOUSING ACC. TO EN50047, 31MM DEVICE CONNECTION 1X(M20X1.5); 1NO/1NC SNAP-ACTION CONTACTS INTEGRATED (NOT REPLACEABLE) PLASTIC PLUNGER CUSTOMIZED

  • Save filter
  • Load filter
  • email on update
33
Entries
Filtered by
'
3SE5232-0HC03-8AA5
'
 
Entries per page: 20 50 100
...
1
2
...
FAQ Diagnostic coverage level to be specified and achievable safety integrity level for subsystems or SRP/CS with electromechanical components

This entry provides information on the diagnostic coverage level.

09/28/2018
ID: 35444114
(4)
FAQ Safety characteristics - B10 values / failure rates of electromechanical SIRIUS products

This entry contains a list of the B10 values / failure rates of electromechanical SIRIUS products

06/29/2018
ID: 109739348
(31)
FAQ B10 values electro-mechanical command and signaling devices, position and safety switches

This entry provides information on the B10 values of electro-mechanical command and signaling devices, position and safety switches.

02/21/2018
ID: 109749119
(0)
FAQ General: Import of EPLAN Electric P8 macros at edz-Format

This entry contains information about import EPLAN Electric P8 macros at edz-Format in EPLAN

12/04/2017
ID: 48074331
(7)
Application example Protective door with spring-loaded interlocking with an S7-1500

To prevent access to the hazard zone of a machine during operation, a protective door is installed and the position of the protective door is monitored. Since overrunning machine components may cause hazards, the protective door is interlocked and can only be opened after the machine is in standstill.

09/08/2017
ID: 21063946
(4)
FAQ Bypassing safety functions with a key-operated switch in the sensor or actuator circuit

This entry provides information on bypassing a safety function with a key-operated switch

08/21/2017
ID: 109742003
(2)
Application example Monitoring a protective door up to PL e / SIL 3 with a fail-safe S7-1500 controller

To prevent access to the danger range of a machine, a protective door is installed. The machine can only be started, if the protective door is closed. If the protective door is opened during operation or if an error is detected, the machine will be shut down safely.

08/18/2017
ID: 21331363
(6)
FAQ Assessment of the effect of wear and tear on the service life of electromechanical devices

This entry contains information on the effect of wear and tear on the service life of electromechanical devices.

05/31/2017
ID: 109747636
(5)
FAQ Power losses / contact resistance for 3SB1 / 3SB2 / 3SB3 / 3SE3 / 3SE5 / 3SU1

This entry contains information about contact resistance for 3SB1 / 3SB2 / 3SB3 / 3SE3 / 3SE5 / 3SU1 units

02/24/2017
ID: 109741643
(0)
FAQ Reductions for command devices 3SB1 / 3SB2 / 3SB3 / 3SU1 and position switches 3SE2 / 3SE3 / 3SE5 when installed at altitudes of between 2000 and 5000 m above sea level

This FAQ contain the statements for reduction the voltage and current depend on the sea level.

02/15/2016
ID: 86661315
(2)
FAQ General: How to order the Product Catalog CA01

This FAQ describe how to order the Product Catalog CA01 on DVD.

07/20/2015
ID: 21656919
(3)
FAQ 3SE / 3SF position switches Hysteresis values when used in safety controllers

This FAQ describe the hysteresis for slow-action and snap-action contacts

06/24/2015
ID: 109474538
(1)
FAQ Certificates of origin, certificates of conformity, test reports, factory certificates for products from the distribution center in Amberg (Lieferzentrum Amberg (LZA)).

QUESTION: Who is responsible for issuing certificates of origin and certificates of conformity (EN 10204-2004-2-1), test reports and factory certificates for products from Amberg (LZA)? ...

01/26/2015
ID: 99684616
(3)
08/06/2014
ID: 35444144
(0)
FAQ Achievable SIL with SIRIUS subsystems or subsystem elements that have a low demand rate according to IEC 61511

QUESTION: What Safety Integrity Level SIL is achievable with SIRIUS subsystems or subs ...

08/06/2014
ID: 35444323
(1)
FAQ PFHD values in the informative annex K, Table K.1 of the ISO 13849-1 standard

QUESTION: ISO 13849-1 – Application Explanations How are the PFHD values in the i...

08/05/2014
ID: 35444036
(0)
FAQ Calculation of “non-electrotechnical components” permissible on the basis of IEC 62061

QUESTION: Why may “non-electrotechnical components”, e.g. valves, also be calculated on the basis of IEC 62061? ...

05/27/2014
ID: 35444396
(0)
FAQ General: Is it mandatory to switch all phases of a 3-phase load?

QUESTION: Is it allowed to switch only 2 phases of a 3-phase load? ...

05/20/2014
ID: 21656588
(0)
FAQ Regulation for protecting switching devices against overload and short-circuits

QUESTION: How must switching devices be protected against overload and short-circui ...

05/19/2014
ID: 91198957
(0)
FAQ Pulling forces for conductors with Cage Clamp connection technology

QUESTION: What pulling forces apply for round copper conductors that are connected to ...

05/13/2014
ID: 21656695
(1)
 
Entries per page: 20 50 100
...
1
2
...