3SF5804-4EB05
SIGNUM 3SB3
PUSHBUTTON IN HOUSING; ASI HOUSING CUSTOMIZED 4 COMMAND POINTS ACC. TO OFFER 47017

  • Save filter
  • Load filter
  • e-mail on update
16
Entries
Filtered by
'
3SF5804-4EB05
'
 
Entries per page: 20 50 100
...
1
...
FAQ Conversion list for phase-out of 3SB3/1/3SF5 to SIRIUS ACT (3SU1)

This entry contains information on converting 3SB3/1/3SF5 to SIRIUS ACT (3SU1)

07/04/2019
ID: 109756490
(1)
FAQ 3RK1 ASIsafe: Recognition of short-time errors (safety component releases for a short time)

QUESTION: How can short-term errors / releases of safety components be recognized? The system remains at a standstill but it is not known which component has released. ...

03/19/2012
ID: 10052281
(0)
FAQ 3SF580 AS-i-enclosures: I/O configuration and ID code

QUESTION: I need the I/O configuration and the ID code for the AS-i-enclosures 3SF580. ANSWER:...

03/12/2012
ID: 21401818
(0)
FAQ 3RK1 ASIsafe: Configuration of the network structure with Safety at Work

QUESTION: Are different investments in the network infrastructure necessary for handling standard and secure data on the AS-Interface? ...

03/08/2012
ID: 12183914
(0)
FAQ 3SF5 PROFIBUS-DP single connection: Arrangement of control devices

QUESTION: How close together can control devices be mounted in the PROFIBUS-DP single connection 3SF5? ...

03/07/2012
ID: 21403794
(1)
FAQ 3SF5 PROFIBUS-DP single connection: Approval for explosion hazardous areas

QUESTION: Are 3SB3 units for PROFIBUS-DP single connection...

03/07/2012
ID: 21403818
(0)
FAQ 3SF5874 AS-i-Front Panel Modules: Do I need a special cable for the addressing?

QUESTION: Do I need a special cable for the addressing of a 3SF5874-4 ...

03/07/2012
ID: 21403577
(0)
FAQ 3SB38/3SF58 enclosures: Material of screws of enclosures

QUESTION: Which material are the screws of 3SB38 and 3SF58 made of? ...

03/02/2012
ID: 26670194
(0)
FAQ 3SB38 enclosures: Metal enclosures for extreme mechanical requirements and screws made of stainless steel

QUESTION: Are there any metal enclosures or stainless steel screws available within 3SB38 product range? ...

08/04/2011
ID: 23158688
(0)
FAQ 3SB3 Pushbuttons and Indicator Lights: Online configurator 3SB3/3SF5

QUESTION: Online configurator for 3SB3/3SF5 Pushbuttons and Indicator Lights ...

04/07/2011
ID: 22793860
(0)
Product note Mall configurator for SIRIUS 3SB3/3SF5 pushbuttons and indicator lights

Mall configurator for SIRIUS 3SB3/3SF5 pushbuttons and indicator lights – the integrated full-range portfolio for all applications. ...

03/25/2010
ID: 41993251
(0)
FAQ 3RK1 ASIsafe: installation guideline for Safety at Work

QUESTION: Are there special installation guidelines for ASIsafe? ANSWER:...

05/07/2007
ID: 25429744
(1)
FAQ 3RK AS-i General: CCC certification for China

QUESTION: Is there a CCC certification for AS-Interface, ASIsafe, AS-i cables for China available ? ...

04/05/2006
ID: 22981142
(0)
FAQ AS-Interface: Behavior of AS-Interface under fault conditions (EMC)

Request : How is the electromagnetic compatibility (EMC) of AS-Interface? Suggestion : Attached you will find some statements about the...

05/17/2001
ID: 7549015
(0)
FAQ Load current of electronic outputs of AS-I modules > 2 A

Request : Under what conditions can the electronic outputs of AS-I modules be loaded with a current greater than 2 A? Mechanical contacts are not permitted for this particular application. Suggestion : The maximum load current is 2 A per electronic output. The summary of all (up to 4) output currents may not exceed 4 A. In an overload condition the current monitoring feature shuts the module down. As a solution for a load current 2,5 A we recommend ...

08/01/2000
ID: 4748673
(0)
FAQ Sporadic slave failure

QUESTION: What could be the reason for sporadic slave failure on the AS-I bus? ...

04/26/1999
ID: 816139
(0)
 
Entries per page: 20 50 100
...
1
...