3TS3600-0AC2
Contactor AC 50/60 HZ, 24 V
Contactor AC 50/60 HZ, 24 V AC3 400 V 45 A 22 kW AUX. contacts: none size 2

  • Save filter
  • Load filter
  • email on update
26
Entries
Filtered by
'
3TS3600-0AC2
'
 
Entries per page: 20 50 100
...
1
2
...
FAQ Diagnostic coverage level to be specified and achievable safety integrity level for subsystems or SRP/CS with electromechanical components

This entry provides information on the diagnostic coverage level.

09/28/2018
ID: 35444114
Certificate General Product Approval, EAC, IVANOVO-CERTIFICATE

EAC-Certificate 3033

08/31/2018
ID: 109755328
Certificate Confirmation, Manufacturer

Radioactive Material in Products A0308

01/10/2018
ID: 109754897
FAQ General: Import of EPLAN Electric P8 macros at edz-Format

This entry contains information about import EPLAN Electric P8 macros at edz-Format in EPLAN

12/04/2017
ID: 48074331
Certificate Confirmation, Manufacturer

Chinese Quality Check Mark A0210

10/20/2016
ID: 109742339
FAQ General: How to order the Product Catalog CA01

This FAQ describe how to order the Product Catalog CA01 on DVD.

07/20/2015
ID: 21656919
FAQ Certificates of origin, certificates of conformity, test reports, factory certificates for products from the distribution center in Amberg (Lieferzentrum Amberg (LZA)).

QUESTION: Who is responsible for issuing certificates of origin and certificates of conformity (EN 10204-2004-2-1), test reports and factory certificates for products from Amberg (LZA)? ...

01/26/2015
ID: 99684616
08/06/2014
ID: 35444144
FAQ Achievable SIL with SIRIUS subsystems or subsystem elements that have a low demand rate according to IEC 61511

QUESTION: What Safety Integrity Level SIL is achievable with SIRIUS subsystems or subs ...

08/06/2014
ID: 35444323
FAQ PFHD values in the informative annex K, Table K.1 of the ISO 13849-1 standard

QUESTION: ISO 13849-1 – Application Explanations How are the PFHD values in the i...

08/05/2014
ID: 35444036
FAQ Calculation of “non-electrotechnical components” permissible on the basis of IEC 62061

QUESTION: Why may “non-electrotechnical components”, e.g. valves, also be calculated on the basis of IEC 62061? ...

05/27/2014
ID: 35444396
FAQ General: Is it mandatory to switch all phases of a 3-phase load?

QUESTION: Is it allowed to switch only 2 phases of a 3-phase load? ...

05/20/2014
ID: 21656588
FAQ Regulation for protecting switching devices against overload and short-circuits

QUESTION: How must switching devices be protected against overload and short-circui ...

05/19/2014
ID: 91198957
FAQ Pulling forces for conductors with Cage Clamp connection technology

QUESTION: What pulling forces apply for round copper conductors that are connected to ...

05/13/2014
ID: 21656695
FAQ Fuses and miniature circuit breakers for the short-circuit protection of auxiliary contacts

QUESTION: What are the consequences if the short-circuit protection of auxiliary co ...

05/08/2014
ID: 21656724
FAQ Behaviour of Low-Voltage switchgear under conditions of very low air pressure or vacuum

QUESTION: What is the behaviour of Low-Voltage switchgear under conditions of very ...

04/04/2014
ID: 21656902
FAQ General: Temperature behavior of Low-Voltage Switchgear inside the control cabinet

QUESTION: What is the maximum permissible temperature on the plastic surface and connections of Low-Voltage Switchgear? ...

07/05/2013
ID: 76401003
FAQ General: Utilization categories of contactors, contactor relays and auxiliary contacts

QUESTION: Where can I find detailed information on utilization categories according IEC 60947-4-1, 3, 5-1 of contactors, contactor relays and auxiliary contacts? ...

06/18/2013
ID: 23712651
FAQ General: NOM approval mark on the Siemens Industrial Control products

QUESTION: What means the NOM marking on the Siemens industrial control products? ...

06/13/2013
ID: 24378166
FAQ General: Difference between earth fault current and earth leakage current

QUESTION: What is the difference between earth fault current and earth leakage current? ...

06/12/2013
ID: 24490178