3UG3534-1AC50
DISCONTINUED PRODUCT
DISCONTINUED PRODUCT DISCONTINUED TYPE MONITORING RELAY, 22.5 MM, MEAS. VOLTAGE = SUPPLY VOLTAGE THRESHOLD. VALUE A. HYSTERESIS, 1 CO, AC/ DC 20...80 V, SCREW TERMINAL REPLACEMENT TYPE: 3UG4633-1AL30

  • Save filter
  • Load filter
  • email on update
21
Entries
Filtered by
'
3UG3534-1AC50
'
 
Entries per page: 20 50 100
...
1
2
...
FAQ Operation of SIRIUS relays in altitudes of up to 5000m above sea level

This FAQ contain the statements for reduction voltage and current depend on the sea level.

02/23/2018
ID: 109478887
FAQ General: Import of EPLAN Electric P8 macros at edz-Format

This entry contains information about import EPLAN Electric P8 macros at edz-Format in EPLAN

12/04/2017
ID: 48074331
FAQ General: How to order the Product Catalog CA01

This FAQ describe how to order the Product Catalog CA01 on DVD.

07/20/2015
ID: 21656919
FAQ Certificates of origin, certificates of conformity, test reports, factory certificates for products from the distribution center in Amberg (Lieferzentrum Amberg (LZA)).

QUESTION: Who is responsible for issuing certificates of origin and certificates of conformity (EN 10204-2004-2-1), test reports and factory certificates for products from Amberg (LZA)? ...

01/26/2015
ID: 99684616
FAQ Achievable SIL with SIRIUS subsystems or subsystem elements that have a low demand rate according to IEC 61511

QUESTION: What Safety Integrity Level SIL is achievable with SIRIUS subsystems or subs ...

08/06/2014
ID: 35444323
08/06/2014
ID: 35444144
FAQ PFHD values in the informative annex K, Table K.1 of the ISO 13849-1 standard

QUESTION: ISO 13849-1 – Application Explanations How are the PFHD values in the i...

08/05/2014
ID: 35444036
FAQ Calculation of “non-electrotechnical components” permissible on the basis of IEC 62061

QUESTION: Why may “non-electrotechnical components”, e.g. valves, also be calculated on the basis of IEC 62061? ...

05/27/2014
ID: 35444396
FAQ General: Is it mandatory to switch all phases of a 3-phase load?

QUESTION: Is it allowed to switch only 2 phases of a 3-phase load? ...

05/20/2014
ID: 21656588
FAQ Regulation for protecting switching devices against overload and short-circuits

QUESTION: How must switching devices be protected against overload and short-circui ...

05/19/2014
ID: 91198957
FAQ Pulling forces for conductors with Cage Clamp connection technology

QUESTION: What pulling forces apply for round copper conductors that are connected to ...

05/13/2014
ID: 21656695
FAQ Fuses and miniature circuit breakers for the short-circuit protection of auxiliary contacts

QUESTION: What are the consequences if the short-circuit protection of auxiliary co ...

05/08/2014
ID: 21656724
FAQ Behaviour of Low-Voltage switchgear under conditions of very low air pressure or vacuum

QUESTION: What is the behaviour of Low-Voltage switchgear under conditions of very ...

04/04/2014
ID: 21656902
FAQ General: Temperature behavior of Low-Voltage Switchgear inside the control cabinet

QUESTION: What is the maximum permissible temperature on the plastic surface and connections of Low-Voltage Switchgear? ...

07/05/2013
ID: 76401003
FAQ General: Utilization categories of contactors, contactor relays and auxiliary contacts

QUESTION: Where can I find detailed information on utilization categories according IEC 60947-4-1, 3, 5-1 of contactors, contactor relays and auxiliary contacts? ...

06/18/2013
ID: 23712651
FAQ General: NOM approval mark on the Siemens Industrial Control products

QUESTION: What means the NOM marking on the Siemens industrial control products? ...

06/13/2013
ID: 24378166
FAQ General: Difference between earth fault current and earth leakage current

QUESTION: What is the difference between earth fault current and earth leakage current? ...

06/12/2013
ID: 24490178
FAQ Define of Diagnostic Coverage and maximum achievable Systematic Safety Integrity for subsystem resp. SRP/CS with electromechanical components

QUESTION: Which Diagnostic Coverage DC can typically define for a subsystem resp. SRP/CS with electromechanical components and which Systematic Safety Integrity is then achievable? ...

01/25/2013
ID: 35444114
FAQ General: Import of EPLAN P8 macros with the extension *.EDZ

QUESTION: The EPLAN P8 macros on the CAx-DVD and online in the CAx shopping cart have the extension *.EDZ. How can import these macros to P8?...

01/11/2013
ID: 57420555
FAQ General: Special tool with which the user can evaluate by itself the MTTF values (Mean time to failure)?

QUESTION: Is there a special tool available with which the user can evaluate by itself the MTTF values (Mean time to failure) for the devices of the SIEMENS „Industrial Controls Catalog IC 10”? ...

12/21/2012
ID: 61454653