6AG4011-1CA12-1JX0
SIMATIC RACK PC IL 40 S V2,
SIMATIC RACK PC IL 40 S V2, PENTIUM 4 2.8 GHZ, HT; 80 GB HDD EIDE; INTERN.; 256 MB DDR SDRAM, (2 X 128 MB), DUAL CHANNEL; 1.44 MB FDD + DVD-ROM/CD-RW; AGP GRAPHICS, ONBOARD; WINDOWS 2000 PROF. MULTI-LANG. (EN, GER, FR, IT, SP), SP4; INTERFACES: 1X LAN (RJ45); 1XGRAPHICS(VGA); 2X SERIAL (COM1, COM2); 1X PARALLEL (LPT); 6X USB 2.0; 2X FRONT; 2X PS/2; AUDIO; POWER CABLE EUROPE

  • Save filter
  • Load filter
  • email on update
19
Entries
Filtered by
'
6AG4011-1CA12-1JX0
'
 
Entries per page: 20 50 100
...
1
...
FAQ Why isn't there an additional driver for a Siemens Raid Controller on the driver disk?

Description: When you install a new version of Windows, additional drivers have to be loaded from the disk for some device components during the installation process. Examples of these device components include: RAID Controller for hard disks SCSI controllers 29160 ...

08/15/2008
ID: 26348983
(0)
FAQ How do you install Microsoft Windows NT on a SIEMENS SIMATIC PC from a Recovery CD?

Description: To install the Windows NT operating system from a Recovery CD it is recommended first to create two FAT16 partitions of 2 GB each on your computer. Refer to Entry ID 14450825 'Partitioning hard disks with FDISK' for partitioning and formatting the drives. ...

02/04/2008
ID: 14472869
(0)
Application example PC-based Automation: Plant Visualization with Visual Basic .NET via the OPC XML-DA Interface

Problem The following application shows you how to operate and monitor an example process, which is controlled by a WinAC RTX controller, using a self-generated visualization user interface. ...

03/30/2005
ID: 21004994
(0)
Manual SIMATIC Rack PC IL 40 S V2

09/2004, Manual, A5E00200171-03

10/04/2004
ID: 19250619
(0)
FAQ Hard disk sizes supported by Siemens Industrial PCs

QUESTION:   Which hard disk sizes are supported by Siemens Industrial PCs? ANSWER:  ...

09/22/2004
ID: 19515714
(0)
FAQ Keyboard lock for WinCC Runtime with SIMATIC Rack PC IL 40 S and IL 40 S V2

QUESTION:   How can I disable the hotkeys of the graphics card (CTRL+ALT+F12, CTRL+ALT+Up Arrow and CTRL+ALT+Down Arrow) for WinCC Runtime with SIMATIC Rack PC IL 40 S and IL 40 S V2? ...

09/17/2004
ID: 19490318
(0)
Manual BIOS Setup V4.06

05/2003, Brochure, A5E00343431

07/22/2004
ID: 19251405
(0)
Manual SIMATIC Rack PC IL 40 S V2 Data Mainboard D1567-C/D1562-C

02/2004, Product information, A5E00343470

07/22/2004
ID: 19250498
(0)
Manual SIMATIC Rack PC IL 40 S V2 Mainboard D1567

12/2003, Manual, A5E00343477

07/22/2004
ID: 19249526
(0)
Manual SIMATIC Rack PC IL 40 S V2 Getting Started

06/2004, Getting Started, A5E00524329-01

07/22/2004
ID: 19250735
(0)
Product note New SIMATIC Rack PC IL 40 S V2 Released for Delivery

The innovated SIMATIC RACK PC IL 40 S is herewith released for delivery. ...

07/01/2004
ID: 19137875
(0)
FAQ Conflict between the internal interface for the memory card and the Ethernet card

QUESTION: What can I do if in Windows NT the internal interface for the memory card no longer functions in conjunction with another PCMCIA network card that is slotted in addition? ...

05/12/2003
ID: 15219831
(0)
FAQ Switching between an onboard and a PCI graphic card

QUESTION: How can I switch from an onboard graphic card to an additionally installed PCI graphic card? ...

03/26/2003
ID: 14897056
(0)
FAQ BIOS password of PC forgotten

QUESTION: I forgot the BIOS password of my SIMATIC PC. How can I erase it or set a new one? ...

12/11/2002
ID: 13964195
(0)
FAQ Removing AutoLogon on Rack PC IL40 in Win 2000

QUESTION: How can I prevent my Rack PC IL40 from logging on automatically as Administrator when starting Windows 2000? ...

11/25/2002
ID: 13706130
(0)
FAQ Changing the keyboard layout of the Windows logon mask

QUESTION: There is always the English keyboard layout enabled in the logon mask of the PC, even though the German keyboard layout has been set after logon. How can I set the keyboard layout of the Windows logon mask? ...

11/05/2002
ID: 13494263
(0)
FAQ Error message when starting Windows: "Cannot find the HKCMD.exe file or one of your components"

QUESTION: How can I clear the following error message I get when starting windows: 'Cannot find the HKCMD.exe file or one of your components'? ...

09/17/2002
ID: 11990107
(0)
FAQ Creating a bootable system floppy disk for BIOS update

QUESTION: How do I create a bootable system floppy disk for a BIOS update? ANSWER:...

08/07/2001
ID: 7239285
(0)
FAQ Definition of terms: FAT file system

QUESTION: What is to be understood by the 'FAT' file system? ANSWER:...

04/17/2001
ID: 7222410
(0)
 
Entries per page: 20 50 100
...
1
...