6AV6371-1DH05-1CX8
WINCC WEB NAVIGATOR V1.2 SP2, 25 CLIENTS
WINCC OPTION WEB NAVIGATOR SERVER AND CLIENT COMPONENTS, W. 25 CLIENT LICENSES VERSION V1.2+SP2 GERMAN, ENGLISH, FRENCH

  • Save filter
  • Load filter
  • e-mail on update
72
Entries
Filtered by
'
6AV6371-1DH05-1CX8
'
 
Entries per page: 20 50 100
...
1
2
3
4
...
FAQ Compatibility Tool for Automation and Drive Technology

The Compatibility Tool is a function provided by the Industry Online Support with which you can select compatible software products or check the compatibility of existing configurations.

09/07/2021
ID: 64847781
(151)
FAQ Which exceptions for hardening measures according to CIS must be made in order to use WinCC WebNavigator?

The connection of systems to the internet has many advantages but also security risks. In order to protect systems, the "Center for Internet Security" (CIS) provides instructions on how to secure systems. This FAQ response lists the exceptions to the hardening measures that must be made to allow a connection between the WinCC WebNavigator server and the client.

01/31/2020
ID: 109773160
(0)
Product note SITRAIN advanced course: WinCC V7 and WinCC Options

Advanced course for WinCC V7 and WinCC options; Product training, Type: Classroom training course; Duration: 5 days; different regions/sites

12/04/2019
ID: 109758660
(0)
Application example Decentralized Operation of SIMATIC WinCC with SIMATIC Thin Clients

This article shows you how you can access using a decentralized Industrial Thin Clients to a WinCC project .

11/19/2015
ID: 28309119
(22)
FAQ How do you parameterize the communication resources of S7-300 CPUs so that WinCC stations and S7-300 stations do not have connection failures?

If you need multiple OS connections to an S7-300, then for the S7-300 you must set the number of connections accordingly in the hardware configuration (HW Config). You need these settings because the communications resources are restricted.

02/16/2011
ID: 23369901
(0)
FAQ With WinCC Web Navigator, how can you have a display of which users are currently accessing the web project?

Description: The 'Status.html' page is for diagnosing the WinCC Web Navigator server and its active connected clients. ...

02/19/2010
ID: 9595381
(2)
FAQ How can I create script functions that are to run on the WinCC Server or WinCC client, but not on the Web Navigator Client?

Description In the following example, the 'DMExitWinCCEx( )' command is executed only when the button on the Web Navigator server is operated, but not when the button is operated on the Web Navigator client.  ...

02/19/2010
ID: 11699740
(0)
FAQ Why do you get the error message "The maximum count of allowed users is connected to the WinCC server"?

Description You are using WinCC V5/SP1 and Web Navigator V1.0 and you get the error message 'The maximum count of allowed users is connected to the WinCC server'. ...

For products: 6AV63.1-....5-...., 6AV6371-1DH05-1...
02/19/2010
ID: 2444186
(0)
FAQ What are the differences between the WinCC Basic System and the WinCC Web Navigator?

Description Attached is the chapter 'Differences to the WinCC Basic System' as a supplement to the Web Navigator documentation V1.2. As of WinCC Web Navigator V6.0 this information is in the 'WinCC Web Navigator - Documentation' under 'Configuring a Web Project' > Differences to the WinCC Basic system > Scripting'. ...

02/19/2010
ID: 11966247
(0)
FAQ Which bandwidth does the WinCC web client need for communications with the WinCC Web Navigator server?

Description: The speed and bandwidth of your access to the Internet on the WinCC Web Navigator has a great influence on the performance of your WinCC projects, picture selection and update times of your WinCC web clients. Each client has a bandwidth requirement of about10 kbps. ...

02/19/2010
ID: 10113139
(0)
FAQ How can you configure an IO field that can be operated on the WinCC server in runtime, but not on the Web Navigator client?

Description To the I/O Field you must add a C script to the attribute 'Operator-Control Enable' (Fig. 1), which with the preprocessor definition #ifdef RUN_ON_WEBNAVIGATOR returns the value 'FALSE' to the Web Navigator client and the value 'TRUE' to the server (WinCC Runtime). ...

02/19/2010
ID: 11870798
(0)
FAQ Why, after migration of a WinCC project from WinCC V5.1 to WinCC V6.0 SP1, is the text originally configured no longer displayed on the Web Navigator client, but only "TEXT" in buttons and in static texts?

Description Contrary to version V5.x, the Web Navigator users of WinCC V6.x are no longer managed in the Web Administrator, but along with other configurable WinCC users in the WinCC User Administrator. Regarding users already created in WinCC V5.1, the migration to V6.0 SP1 causes a loss of allocations between user and configured language, thus resulting in displaying the text as 'TEXT'.  ...

02/15/2010
ID: 18946449
(0)
FAQ How do you set the user rights for the WinCC Web Navigator?

Procedure for WinCC Web Navigator V6.0 As from WinCC Web Navigator V6.0 you manage user rights in the WinCC User Administrator. A detailed description is available in the WinCC Web Navigator documentation, in the chapter entitled 'Configuring User Administration'. ...

02/15/2010
ID: 6727600
(0)
FAQ How can you prevent an empty page being displayed when you call the diagnostics information saved by the WinCC Web Navigator from the STATUS.HTML page?

Description If you have saved the STATUS.HTML page from the Internet Explorer using 'File > Save as > Web page, complete (*.htm,*.html)' and you then open this, the display is empty. ...

02/15/2010
ID: 19244541
(0)
FAQ Is the " ProgramExecute" function supported on the Web Navigator client?

Description: The 'ProgramExecute' function is supported on the Web Navigator client as long as the file to be executed is also locally on the Web Navigator client. Furthermore, the file must be in the same directory as on the Web Navigator server. ...

02/15/2010
ID: 8956826
(0)
FAQ What causes the error message "Network request not supported" when starting the client Web Navigator site from the IIS?

Description In the Internet Service Manager (for Windows NT Workstation) or Internet Information Service (for Windows NT Server) on the WinCC server you want to start the website for the Web Navigator client  and you get the error message: 'Network request not supported'. ...

For products: 6AV63.1-....5-...., 6AV6371-1DH05-1...
02/12/2010
ID: 8275734
(0)
FAQ Why is the "Close" button of a picture window not visible on the WinCC Web Navigator client?

Initial situation: Contrary to the display of a picture window in WinCC Runtime, the 'Close' button of the picture window is not displayed on WinCC Web Navigator V1.2 although the 'Can Be Closed' property is configured with 'Yes' ('Properties > Miscellaneous'). ...

For products: 6AV63.1-....5-...., 6AV6371-1DH05-1...
02/09/2010
ID: 11869808
(0)
FAQ What are the requirements for installing the Microsoft IIS (Internet Information Server) for the WinCC Web Navigator V1.x on a Microsoft NT Workstation?

Description In order to be able to apply the Microsoft Internet Information Server (IIS) on a Microsoft Windows NT Workstation, you must have the 'Internet Service Manager' installed. Proceed as follows: ...

For products: 6AV63.1-....5-...., 6AV6371-1DH05-1...
02/04/2010
ID: 5895676
(0)
FAQ What known statuses can a computer assume when you reinstall the WinCC Web Navigator V1.1 and what do these statuses mean?

Description There are three known system statuses when a web server is installed and they indicate the following: When reinstalling the Web Server, The Setup remains unchanged when you reinstall the web server. ...

For products: 6AV63.1-....5-...., 6AV6371-1DH05-1...
02/04/2010
ID: 8954813
(0)
FAQ Are the web clients not updated although the web server has been updated with a new client package?

Description It might be that the page http://computername/PROJECT.ASP is called directly in the client browser although the call has been stored in your browser as favorite/bookmark. This is the case if you have used the IE function 'Add to Favorites'.  ...

For products: 6AV63.1-....5-...., 6AV6371-1DH05-1...
02/04/2010
ID: 10811061
(0)
 
Entries per page: 20 50 100
...
1
2
3
4
...