6AV7612-0AA12-0CE0
PANEL PC 670 12 TOUCH WIN98 D
SIMATIC PANEL PC 670 12" TF TOUCH DISPLAY, 20 GB HD, 64 MBYTE RAM, CPU PENTIUM III 500 MHZ, 115-230V EUROP. SYSTEM CABLE, WIN98 GERMAN

  • Save filter
  • Load filter
  • email on update
23
Entries
Filtered by
'
6AV7612-0AA12-0CE0
'
 
Entries per page: 20 50 100
...
1
2
...
Application example Loading a PC Station via configuration file import

Load a PC Station via configuration file import without a connected TIA portal via *.psc-file.

07/27/2018
ID: 109759142
(0)
FAQ How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this?

Description The document attached for downloading contains information on the topic of ...

08/19/2011
ID: 19142034
(1)
FAQ How do you make printouts on different printers in WinCC flexible PC Runtime?

Instructions In WinCC flexible PC Runtime you cannot explicitly specify printers for printouts. All printouts from the WinCC flexible PC Runtime are always output on the default printer set in Windows. ...

04/27/2011
ID: 49741726
(1)
FAQ Which program changes have to be made in an S5 controller if a line or graphics operator panel with PROFIBUS connection is replaced by a Windows-based operator panel?

Configuration Notes: If you wish to exchange a line or graphics operator panel, which is connected to a SIMATIC S5 controller via a PROFIBUS DP link, for a Windows-based operator panel, this necessitates the program changes described below. ...

11/27/2009
ID: 31676209
(0)
Product note Information on the Total Discontinuation of the Panel PC 670 (V1) 6AV761

The SIMATIC Panel PC 670 (V1) has been totally discontinued since 10/01/2007.  We would like to point out that repairs to HMI devices are still possible even after the date of the total discontinuation. For this, please directly contact the SIMATIC PC Repair Center. ...

09/02/2008
ID: 30816153
(1)
FAQ How can you calculate the actual local time (summer time or winter time) in the S7-300/400 CPU and then use it on the panel as system time?

There is no time conversion of the S7-300/400 CPU clock to summer or winter time in automation facilities with integrated time synchronization.

08/15/2008
ID: 19324378
(0)
FAQ How can you use an English operating system with a German keyboard without having to worry about the z and y keys?

Description: You have installed an English operating system on your computer. Upon installation it was assumed that you are using an American keyboard. However, you want to use a German keyboard. This leads problems when logging on and above all when entering the password. You must make sure that you use the z key instead of the y key and vice versa. Once you have logged on, you can create your own configuration with the correct keyboard definiti ...

03/12/2008
ID: 902013
(0)
FAQ How is the connection between a Windows-based panel and a SIMATIC S5 set up?

Instructions: SIMATIC HMI Windows-based panels do not possess a TTY (20mA) interface which is needed for communication with a SIMATIC S5 PLC. ...

02/07/2008
ID: 21923974
(1)
FAQ Which settings do you have to make on the TS Adapter IE to transfer a ProTool project via Teleservice?

Configuration Notes: Using the TS Adapter IE (TSA-IE), you can transfer the configuration of a panel or Runtime PC connected to an Ethernet network via the telephone network. ...

12/18/2007
ID: 27153767
(0)
FAQ How do you switch an operator panel to transfer mode when the autostart's timeout is set to 0 seconds?

Instructions:   No. Procedure 1 If 'Zero Seconds' is set for the delay time ('Autostart' or 'Startup Delay') when the operator panel is started, then the operator panel starts with the corresponding Runtime configuration directly after booting. ...

12/17/2007
ID: 23034454
(0)
Application example WinCC flexible 2005: Accessing a Panel via an HTML Page Supported by Sm@rtAccess

Problem:   Your customer has different plant sections that are operated via several multi panels. ...

08/23/2007
ID: 26331265
(0)
FAQ How can I acknowledge alarms in WinCC flexible via the PLC?

Instructions: Proceed as follows to acknowledge error messages via the controller. ...

03/16/2007
ID: 19439876
(0)
FAQ How do you simulate the system keyboard via K or F-keys?

Instructions: The system keyboard can be simulated using the SimulateSystemKey function from WinCC flexible 2005. The function is particularly useful if the operator panel does not possess a separate number block or if, for example, you use an OP177B with a touch/button combination. ...

12/13/2006
ID: 24259526
(1)
FAQ Tips and tricks for creating faceplates

Is multiplexing possible with structure tags? With WinCC flexible it is not possible to multiplex structure tags. ...

11/10/2006
ID: 24171755
(0)
FAQ How do you configure a PROFINET connection to an S7 controller in WinCC flexible?

Instructions: The PROFINET IO is based on the Industrial Ethernet. If, for instance, you wish to use PROFINET communication for Mobile Panel 277, you will need to configure 'Ethernet communication' in the configuration interface via 'Communication > Connections'. ...

10/06/2006
ID: 23991461
(0)
Application example WinCC flexible: Engineering with Recipes Using Integrated Functionalities

Problem:   This application was created to provide you with information on “engineering with recipes”. show the different setting options for the recipe parameters and how they affect the running process. ...

09/28/2006
ID: 23901413
(3)
FAQ How high are the MTBF (Mean Time Between Failure) values for the SIMATIC Panel PCs 677 and 877?

Description: MTBF means Mean (Operating) Time Between Failure. There is a common misunderstanding that the MTBF is the expected minimum - guaranteed - service life (or time to failure) of parts and devices. ...

06/26/2006
ID: 23493978
(0)
FAQ How do you operate an external monitor in Dual Display Mode on the Panel PC IL 77?

Instructions: Operation with an external monitor only is already described in the manual for the Panel PC IL 77 (Entry ID 19768660) Panel PC 577 (Entry ID 22216685) ...

11/28/2005
ID: 21497278
(0)
FAQ Difficulties when Shutting Down Windows 98 Second Edition

QUESTION:   Why does Microsoft Windows 98 SE stop during shut down with the message 'Your Computer will be shut down'? ...

08/12/2004
ID: 19341682
(0)
Manual SIMATIC PC Panel PC 670/870 Operating Unit

07/02, Manual

06/27/2002
ID: 2169187