6ES7157-0AD00-0XA0
DP/PA COUPLER, EX-VERSION
SIMATIC DP, DISTRIBUTED I/O DP/PA COUPLER EX-VERSION FIELD BUS COUPLER BETWEEN PROFIBUS-DP AND PROFIBUS PA DEGREE OF PROTECTION IP20

  • Save filter
  • Load filter
  • email on update
35
Entries
Filtered by
'
6ES7157-0AD00-0XA0
'
 
Entries per page: 20 50 100
...
1
2
...
Manual Catalog ST PCS 7 (system components) SIMATIC PCS 7 for V9.0

2017, Catalog, E86060-K4678-A111-C5-7600, E86060-K4678-A111-C5-7600

04/16/2018
ID: 109745632
(1)
Certificate General Product Approval, China-RoHS, Manufacturer

SIMATIC PCS7 - Information for Hazardous substance restrictions identification marking (SJ/T 11364-2014)

08/29/2017
ID: 109738803
(1)
FAQ What is the difference between the PROFIsafe address types 1 and 2 in relation to the uniqueness of the PROFIsafe address?

The PROFIsafe address is for the unique addressing of the F IO and for protecting standard address mechanisms like IP addresses. Here, the uniqueness is defined differently with the F IO of the PROFIsafe address type 1 and with the F IO of the PROFIsafe address type 2. The differences are explained below.

06/16/2016
ID: 109479905
(10)
Manual Brochure - IO-Link for transparency down to the lowest field level

Simple wiring, fast fault diagnostics, efficient engineering

03/01/2015
ID: 109750215
(0)
Application example PROFIBUS: Field Automation with PROFIBUS in the process industry

Problem For PROFIBUS DP/PA there are a number of possibilities for mechanical and electronical setup, for connecting PROFIBUS networks, as well as for communication with analog input and output modules and field devices. For the beginner in particular it is difficult to get a quick overview over ...

04/22/2014
ID: 21602560
(0)
Manual SIMATIC Field Automation with PROFIBUS in the Process Industry

04/2005, System manual

04/07/2014
ID: 90880058
(2)
FAQ How do you connect the IM 157/IM 153-2 in the DP/PA Link to an external master or a SIMATIC S5? (GSD tool)

Instructions In order to be able to evaluate values from PROFIBUS PA devices on PROFIBUS external masters (ABB or SIMATIC S5, for example), the address areas of these devices must be known in the DP/PA Link. The GSD tool facilitates configuring in that one single GSD file is generated on the external masters from the GSD file of the IM 157 (6ES7157-0AA82/81-0XA0) or IM 153-2 High Feature (6ES7153-2BA81/82-0XB0) in the DP/PA Link and the GSD files of the PROFIBUS PA field devices. ...

09/04/2013
ID: 26562190
(5)
Manual SIMATIC Process Control System PCS 7 Released Modules (V7.1 SP3)

05/2011, Product information, A5E02124692-03

08/30/2013
ID: 79719965
(1)
Certificate General Product Approval, UL, UL

UL-Listing Canada: "Programmable Controllers " E248953

01/22/2013
ID: 27840279
(0)
FAQ How do you configure an S7-300 CPU or a CP342-5 as DP slave to an S7-400H as DP master using a Y-link?

Description This entry describes how to configure a CPU 417-4H as DP master. Via a Y-link you connect an S7-300 CPU and a CP342-5 as DP slaves to the redundant DP master system of the CPU 417-4H. Furthermore, this entry describes how to program the data exchange between DP master and DP slave. ...

09/19/2011
ID: 19951154
(1)
FAQ How do you assign the PA address when the DP/PA link has been configured via GSD file?

Instructions: The GSD file is needed, if you intend to insert a DP/PA link into COM PROFIBUS or into the configuration tool of a third-party master. The PA slaves are then configured as slots in the configuration model of the DP/PA link. ...

12/17/2007
ID: 22729489
(0)
FAQ Why can't you connect PA slaves directly to an interface for PROFIBUS DP slaves?

Description: PROFIBUS PA slaves can only be connected to a DP/PA coupler or to a DP/PA link/coupler combination. ...

12/17/2007
ID: 22729521
(0)
Manual Configuration and parameter assignment frame for the DP/PA link

03/06, Product information, A5E00190399-03

08/16/2006
ID: 13406349
(1)
FAQ How many DP/PA couplers can be operated after a DP/PA link?

  Configuration notes: You can operate up to five DP/PA couplers after a DP/PA link....

03/14/2006
ID: 22729070
(0)
FAQ What options are there for diagnosing slaves on the PROFIBUS PA?

    Configuration notes:...

03/14/2006
ID: 22730197
(1)
FAQ Why doesn't the PA bus run (LED PA doesn't light) although there is no fault on the DP side?

    Description:...

03/14/2006
ID: 22731508
(0)
FAQ Behavior of the DP/DP coupler when a master system fails

QUESTION:   How do I recognize failure of a DP master on the other side of the DP/DP coupler?  ...

02/02/2005
ID: 18852586
(1)
FAQ Configuring I/O addresses with DP/AS-i Link 20E

QUESTION:   Can I configure different input and output addresses with the DP/AS-I Link 20E? ...

12/16/2004
ID: 19992394
(0)
FAQ Configuration of the I/O Data on DP/DP Coupler

QUESTION:   Why does the DP/DP coupler (6ES7 158-0AD0x-0XA0) not go into the faultless operation, although the sum of all I/O data was seemingly configured correctly on both sides? ...

08/03/2004
ID: 19281019
(0)
FAQ Reading the input data of a DP slave configured by a different DP master

QUESTION:   Can a DP master read the input data of a DP slave configured by a different DP master? ...

06/21/2004
ID: 19081112
(0)
 
Entries per page: 20 50 100
...
1
2
...