×
Siemens Industry Online Support
Siemens AG
Filter criteria for entries
All Products
My Products
Product tree
 
 
Clear all filters
Product
Search product
Entry type
 
Date
Thumbnail
CPU314IFM, 16DI/DO, 4AE, 1AA, 24KB
SIMATIC S7-300, CPU 314 IFM COMPACT CPU WITH MPI, 16DI/16DO, 4AI/1AO, 2 X 40 PIN, INTEGRATED 24V DC POWER SUPPLY, 24 KBYTE WORKING MEMORY
  • Save filter
  • Load filter
  • e-mail on update
266
Entries
Filtered by
'
6ES7314-5AE00-0AB0
'
 
Entries per page: 20 50 100
...
1
2
3
4
5
...
FAQ How do you find the right successor product if the existing product has already been discontinued?

In the following, you will find instructions on how to replace the discontinued module and determine compatibility information.

12/09/2021
ID: 109804833
(0)
FAQ Why is the value of a string variable from a SIMATIC S7-300 controller not displayed in WinCC Unified RT?

So that the value of a S7-300 string can be displayed in WinCC Unified Runtime, the length of this string data type must be specified in the corresponding S7-300 data block.

12/06/2021
ID: 109804131
(1)
Application example Function blocks and faceplates for evaluation of the diagnostic interface "COM" of the SITOP PSU6200 and visualization of the device data

The SITOP PSU6200 power supply has a diagnostic interface "COM" whose signal can be evaluated via a digital input in a higher-level controller, e.g. S7-1200 CPU, S7-1500 CPU and S7-300 CPU / S7-400 CPU.

11/19/2021
ID: 109760217
(8)
FAQ How are the variables stored in the temporary local data?

In the following we explain the local data addressing with S7-300/S7-400.

07/28/2021
ID: 291495
(1)
Application example SITOP UPS1600: Faceplates and Communication Blocks (TIA Portal, STEP 7 and WinCC)

Use the prepared and handy faceplates and function blocks of this application example in order to connect the uninterruptible SITOP UPS1600 power supply to your plant. Furthermore, you can find out how you can shut down your plant in a defined state for longer power failures and how to secure process values.

07/13/2021
ID: 78817848
(26)
Certificate General Product Approval, China-RoHS, Manufacturer

Statement to China-RoHS directive for SIMATIC ( Panel, ITC, IPC, PG, ET200x, S7-xx, LOGO!, Cables, Network Compontents... ) China-RoHS SIMATIC all V1.7

07/08/2021
ID: 109738555
(6)
FAQ Implementation of SIMATIC modules in environments with high concentrations of corrosive gas

SIMATIC modules of the product families S7-300, S7-400, S7-1500, ET 200M, ET 200S, ET 200SP, ET 200SP HA, ET 200MP, ET 200iSP, TDC are also approved for implementation in environments with high concentrations of corrosive gas in compliance with ISA–S71.04 severity level G1; G2; G3. ...

07/07/2021
ID: 28569857
(3)
Application example Integration of third-party Systems with SIMATIC PCS 7/OPEN OS

Today's process engineering systems are often made up of system landscapes that have grown over many years and include control systems from different manufacturers. The main challenge is to integrate various systems from different manufacturers into one operator control and monitoring system. The automation system that is responsible for the sensors and actuators is of secondary importance.

06/23/2021
ID: 49740087
(8)
FAQ Where can you find the latest updates of the operating systems for the CPUs S7-31x, IM15x and BM147?

Overview of the firmware versions of all S7-300 CPUs

04/28/2021
ID: 26290163
(5)
FAQ Why does the message "16# 4546 STOP caused by CPU memory management” appear in the diagnostics buffer with an S7-300 CPU?

You get this message in the diagnostics buffer of STEP 7 (TIA Portal) if the S7-300 CPU recognizes an access error to the MMC.

10/12/2020
ID: 109782017
(2)
Certificate Declaration of Conformity, UL, UL

UL Certificate of Compliance for Programmable Controllers Simatic System S7-300 or SPPA-T3000 No. E116536 (English) E116536

08/17/2020
ID: 109775198
(0)
FAQ Where can you find certificates and approvals for SIMATIC S7 on the internet?

Certificates and approvals are available on the Siemens Service and Support pages.

05/04/2020
ID: 42745
(4)
FAQ Why does the S7-300 station not start up with Ethernet or PROFIBUS CP?

There are several reasons why the S7-300 station will not start up with Ethernet or PROFIBUS CP.

04/23/2020
ID: 18381922
(0)
Certificate Marine / Shipping, CCS / China Classification Society, CCS (China Classification Society)

China Classification Society (CCS) Approval of the SIMATIC Systems S7-300/M7-300 HB20PTB00004_12

03/02/2020
ID: 42717867
(2)
Application example FTP communication with S7-300/400

The File Transfer Protocol (FTP) is one of the classic, standardized options of exchanging data with PCs or any heterogeneous computer system. This entry shows how FTP communication is realized in a SIMATIC S7-300/400 station. ...

02/11/2020
ID: 21605954
(4)
Application example Migration Guide: SIMATIC S7-300/400 to SIMATIC S7-1500

This migration guide contains recommendations and notes for users who are currently using SIMATIC S7-300/400 automation systems and plan to migrate to the new SIMATIC controller generation S7-1500.

12/09/2019
ID: 109478811
(23)
Application example SIMATIC/SIMOTION Weihenstephan Standards

This application supports in integrating the Weihenstephan Standards into SIMATIC controllers and the motion control system SIMOTION. The Weihenstephan Standards (WS) define a universal communication interface for connecting machines to higher level data acquisition systems or MES (Manufacturing Execution systems). They also define the data which must be provided for acquisition.

11/14/2019
ID: 109475571
(6)
Application example SIMOTION, SIMATIC: Communication Library LCom for Ethernet Communication

In the field of automation, the TCP protocol based on Industrial Ethernet is typically deployed for safe, time non-critical (> 25 ms) and multi-system communication.

10/11/2019
ID: 48955385
(21)
FAQ How do S7-300/S7-400/S7-1500 modules behave with CPU RUN/STOP transitions when taken out of the process image?

When the operating mode changes from STOP to RUN, with the S7-1500 the substitute values fail and the values of the output modules flicker.

10/07/2019
ID: 69063762
(2)
FAQ Are SIMATIC controllers free of silicone?

The S7-300/S7-400 and the S7-1200/S7-1500 SIMATIC controllers are free of silicone releases (in the specified operating temperature range).

09/03/2019
ID: 109770478
(1)
 
Entries per page: 20 50 100
...
1
2
3
4
5
...