×
Siemens Industry Online Support
Siemens AG
Filter criteria for entries
All Products
My Products
Product tree
 
 
Clear all filters
Product
Search product
Entry type
 
Date
Task
Thumbnail

6ES7317-2FK14-0AB0
CPU317F-2 PN/DP, 1.5 MB
SIMATIC S7-300 CPU317F-2 PN/DP, Central processing unit with 1.5 MB work memory, 1st interface MPI/DP 12 Mbit/s, 2nd interface Ethernet PROFINET, with 2-port switch, Micro Memory Card required

  • Save filter
  • Load filter
  • email on update
253
Entries
Filtered by
'
6ES7317-2FK14-0AB0
'
and
'
FAQ
'
 
Entries per page: 20 50 100
...
1
2
3
4
5
...
FAQ What remedies are available if the IO controller detects sporadic, transient failures of the IO device?

Sporadic, transient (approx. 1s) failures of PROFINET IO devices produce the following message in the diagnostics buffer of the IO controller:

10/21/2019
ID: 109771776
(1)
FAQ How do S7-300/S7-400/S7-1500 modules behave with CPU RUN/STOP transitions when taken out of the process image?

When the operating mode changes from STOP to RUN, with the S7-1500 the substitute values fail and the values of the output modules flicker.

10/07/2019
ID: 69063762
(2)
FAQ Are SIMATIC controllers free of silicone?

The S7-300/S7-400 and the S7-1200/S7-1500 SIMATIC controllers are free of silicone releases (in the specified operating temperature range).

09/03/2019
ID: 109770478
(1)
FAQ Which modules support the "S7 Routing" function in S7 subnets?

This entry shows which modules support the "S7 Routing" function in S7 subnets to be able to operate cross-network PG/OP communication through S7 Routing.

08/01/2019
ID: 584459
(4)
FAQ Information about product-related environmental protection

Validity: Products of the Operating Company DI (Digital Industries) and Business Unit SI CP (Control Products) of Siemens AG.

06/17/2019
ID: 39200038
(19)
FAQ Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, clock-synchronized mode and option handling?

An overview shows which PROFINET functions you can configure in STEP 7 (TIA Portal) for the PROFINET IO controllers and IO devices.

04/23/2019
ID: 102325771
(9)
FAQ What do you have to do if, after adding a CP or an FM module, the SIMATIC S7-300 CPU no longer switches to RUN mode?

After adding a CP or an FM module, the SIMATIC S7-300 CPU no longer switches to RUN mode but remains in STOP mode.

10/19/2018
ID: 22410800
(0)
FAQ What properties, advantages and special features are offered by the protocols TCP, ISO-on-TCP, UDP and ISO Transport?

An overview shows the properties, advantages and special features of the protocols TCP, ISO-on-TCP, UDP and ISO Transport.

08/08/2018
ID: 26171811
(6)
FAQ What options are available in STEP 7 (TIA Portal) for uploading when the project version in the CPU no longer matches the version on your PG/PC?

Use the functions in the "Online" menu if you want to download the project data from the device to your programing device.

06/22/2018
ID: 97554052
(22)
FAQ Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) with topological configuration and device replacement without topological configuration?

Automatic commissioning (device replacement without interchangeable medium) with topological configuration and device replacement without topological configuration?

05/16/2018
ID: 36752540
(9)
FAQ How do you read out the status of an MRP ring in the user program of the CPU in STEP 7 (TIA Portal)?

There are two ways of reading out the status of an MRP ring in the user program of the CPU.

05/02/2018
ID: 109483240
(12)
FAQ Which IO controllers and IO devices support the following functions in STEP 7 V5.x: IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, I device, sochronous mode, System redundancy and Option handling?

In an overview is shown which PROFINET functions are supported by the PROFINET IO controllers and IO devices in STEP 7 V5.x.

03/15/2018
ID: 44383954
(3)
FAQ How do you save the service data from the CPU in a file in STEP 7 (TIA Portal) and via the web server?

In addition to the contents of the diagnostics buffer the service data of the S7-300/S7-400/S7-1500/ET 200SP CPUs (including CPU 1516 Pro-2 PN) includes further information about the internal status of the CPU.

01/11/2018
ID: 109750782
(1)
FAQ How do you configure open IE communication via the integrated PN/IE interface of the CPU or via an Industrial Ethernet CP?

The properties of the open IE communication via the integrated PN/IE interface of the CPU and via Industrial Ethernet CP are explained below.

10/10/2017
ID: 24294554
(5)
FAQ What should you watch out for when selecting the operating mode in conjunction with functional safety?

When selecting the operating mode in conjunction with functional safety there are often questions about what you should watch out for in this case. What aspects of selecting the operating mode concern functional safety at all? Questions such as these can best be answered using practical examples and also include statutory requirements and compliance with standards.

09/26/2017
ID: 89260861
(10)
FAQ How do you incorporate the execution times of the F blocks for the Mobile Panel 277F IWLAN and 2nd Generation in the S7fcotia table and the S7 Safety Reaction Time Table?

You can use different Excel tables for calculating monitoring and response times in a safety-related application with Distributed Safety and STEP 7 Safety. They can be used to estimate the execution times of the F blocks for the Mobile Panel 277F IWLAN and 2nd Generation.

09/14/2017
ID: 27097159
(4)
FAQ Which ports are used by the various services for data transfer via TCP and UDP and what should you watch out for when using routers and firewalls?

The various services each use their own port for data transfer via TCP and UDP.

07/05/2017
ID: 8970169
(23)
FAQ Configuration examples for unique network-wide and CPU-wide PROFIsafe addresses

Various plant configurations have different requirements for the network-wide and CPU-wide uniqueness of PROFIsafe addresses. This document explains the requirements taking different configuration examples.

06/12/2017
ID: 109740240
(11)
FAQ Comparison: How are the communication resources managed in the S7-300 and S7-1500?

Management of the communication resources of a SIMATIC depends on the type of controller. With the S7-300 you have to respect a number of details before determining the maximum number of devices you can connect for the configuration. The communication management of the S7-1500 has simpler regulations.

06/12/2017
ID: 109747092
(4)
FAQ Which modules of the Siemens portfolio support PROFIenergy functions?

In production sites, breaks occur consistently. With PROFIenergy you can turn off specific consumers that are not needed during the break and in this way significantly reduce energy costs.

05/02/2017
ID: 95848378
(5)
 
Entries per page: 20 50 100
...
1
2
3
4
5