×
Siemens Industry Online Support
Siemens AG
Filter criteria for entries
All Products
My Products
Product tree
 
 
Clear all filters
Product
Search product
Entry type
 
Date
Task
Thumbnail

6ES7331-7KF02-0AB0
SM331, 8AI, 9/12/14Bit
SIMATIC S7-300, Analog input SM 331, isolated, 8 AI, Resolution 9/12/14 bits, U/I/thermocouple/resistor, alarm, diagnostics, 1x 20-pole Removing/inserting with active backplane bus

  • Save filter
  • Load filter
  • email on update
35
Entries
Filtered by
'
6ES7331-7KF02-0AB0
'
and
'
FAQ
'
 
Entries per page: 20 50 100
...
1
2
...
FAQ How do you download the 3D, CAx and ePLAN data for the SIMATIC products?

You can use the CAx download manager to access the latest product data for your CAD or CAE system.

09/20/2018
ID: 89671877
(2)
FAQ Why do you need a compensating box for connecting thermocouples to the analog modules SM331 (6ES7331-7KF02-0AB0 and 6ES7331-7KB02-0AB0) and how do you connect it?

Compensating boxes are used for performing temperature measurements with thermocouples on analog modules. Compensating boxes are needed whenever there is a transfer from the thermocouples to a copper wire via a terminal strip.

04/27/2017
ID: 18272332
(4)
FAQ Information about product-related environmental protection

Validity: Products of the divisions DF (Digital Factory) and PD (Process Industries and Drives) of Siemens AG.

08/04/2016
ID: 39200038
(15)
FAQ How do you standardize and destandardize analog values with STEP 7 (TIA Portal)?

Contrary to binary signals, analog signals take any number of values within a specific range. You have to convert or standardize and destandardize the analog values before you can process, display or output them.

07/04/2016
ID: 77316903
(16)
FAQ How many ET 200M bus modules can you mount on a deep ET 200M mounting channel?

The number of ET 200M bus modules you can mount on an ET 200M mounting channel depends on the following:

04/13/2016
ID: 109483722
(4)
FAQ How do you operate an ET 200M IM 153-2BAx1/-2BAx2 on a redundant ABB system, the AC800M?

The ABB system does not fully support the standard redundancy in accordance with "Specification Slave Redundancy V1.2, Nov. 2004 by the PROFIBUS User Organization; Order No: 2.212".

04/12/2016
ID: 24220825
(2)
FAQ What should you watch out for with S7 analog input modules when measuring temperatures using the degrees Fahrenheit unit instead of degrees Celsius or Kelvin?

The error limits for temperature measurements in the manual are specified for the units degrees Kelvin and Celsius. There is a deviation for the unit degrees Fahrenheit.

10/23/2015
ID: 17376496
(1)
FAQ How do you find the UL certificates for SIMATIC modules?

The following instructions show you how to find the UL certificate on our Support pages taking the example of an S7-1500 digital input module (article number: 6ES7 521-1BL00-0AB0).

10/19/2015
ID: 102840331
(3)
FAQ SINAMICS S120, CU310-2 PN, CU320-2 PN: Maintenance request when allocating NameOfStation

Maintenance request when allocating NameOfStation. The MAINT LED of the CPU lights up yellow.

07/22/2015
ID: 109478287
(2)
FAQ Why do you not have the measuring range of 0…10V with the analog input modules of the S7-1500?

Description With the S7-1500 modules was decided to leave out the measuring range of 0…10V to simplify parameterization. This omission causes no disadvantages from the user's point of view as shown in the comparison below. ...

01/08/2015
ID: 99742113
(1)
FAQ What are the operational limits and the basic errors of analog inputs and outputs?

The most important values for determining the accuracy of analog modules are explained.

07/28/2014
ID: 26116994
(4)
FAQ Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas

SIMATIC modules of the product families S7-300 S7-400 ET 200M ET 200S ET 200iSP TDC are also approved for implementation in environments with high concentrations of corrosive gas in compliance with ISA–S71.04 severity level G1; G2; G3. ...

03/26/2013
ID: 28569857
(2)
FAQ What is a hardware interrupt and how do they work in the S7-300 system?

Instructions: Events can occur in the current process which require responses which are quicker than are possible in the current program cycle. Events also occur which do not last long enough to be identified in the current program cycle. Therefore, there is hardware interrupt processing in SIMATIC S7-300 controllers. ...

12/20/2010
ID: 23657941
(3)
FAQ Why are sporadically not all the modules parameterized when starting up a software redundancy configuration with 2 IM 6ES7153-2BA..-....?

Description When implementing a software redundancy configuration with two IM 6ES7153-2BA..-.... (hereinafter call IM), it might happen that when both IMs are switched on at the same time not all the modules (SM3xx, FM3xx, CP3xx, etc., hereinafter called IO) are not parameterized when the IMs are started up. ...

11/26/2010
ID: 46802313
(0)
FAQ What should you pay attention to when an RTD encoder with 4-conductor connection is connected to an to the SM331 analog input module?

This entry describes how a RTD encoder (4-conductor connection) is linked to the following analog input blocks: SM331 6ES7 331-1KF00-0AB0 SM331 6ES7 331-1KF01-0AB0 SM331 6ES7 331-1KF02-0AB0 SM331 6ES7 331-7KF00-0AB0 SM331 6ES7 331-7KF01-0AB0 SM331 6ES7 331-7KF02-0AB0 SM331 6ES7 331-7KB02-0AB0 SM331 6ES7 331-7PF00-0AB0 SM331 6ES7 331-7PF01-0AB0 ...

11/17/2010
ID: 18839753
(3)
FAQ Which front connector do you need for S7-300 analog/digital modules and for S7-300 compact CPUs?

Description Attachment 1 here gives an overview of the different front connectors for signal modules of SIMATIC S7 300. From the tables you can quickly see which front connector is available for which signal group. ...

05/25/2010
ID: 23060726
(0)
FAQ How should you change the hardware configuration when a 6ES7331-7KF01-0AB0 or 6ES7331-7KF00-0AB0 is configured, but a 6ES7331-7KF02-0AB0 is being used?

Description There is no need to change the hardware configuration, because the 6ES7331-7KF02-0AB0 is the compatible successor module to 6ES7331-7KF01-0AB0 and 6ES7331-7KF00-0AB0 . ...

04/14/2010
ID: 8928766
(0)
FAQ Why, after powering up the CPU or after changing a module, do you get an I/O access error to the analog module 6ES7331-7KF02-0AB0 and 6ES7331-7KB02-0AB0?

Description If you are using the following S7 components in a two-line configuration IM365 (6ES7 365-0BA01 product release 1) 6ES7331-7KF02-0AB0 (product release 4 or 5) 6ES7331-7KB02-0AB0 (product release 4 or 5) ...

04/14/2010
ID: 891333
(0)
FAQ What should you watch out for when using a resistance thermometer that is not in compliance with DIN standards?

Description The S7 analog modules can convert the values of resistance thermometers, e.g. NI 1000, in compliance with DIN 43760. If a different standard is taken, e.g. TC 5000, you have to convert the characteristic. ...

03/22/2010
ID: 18576987
(0)
FAQ How can you avoid measured value fluctuations at high temperatures when using infrared ceramic radiators?

Description: The conductivity of ceramic materials changes at a temperature of 400°C to 600°C and higher. This leads to temporarily higher differences in potential at the heating elements used and to measured value corruption in conjunction with potential-linked analog input modules with a low permissible common-mode voltage. ...

08/26/2009
ID: 17444941
(0)
 
Entries per page: 20 50 100
...
1
2