×
Siemens Industry Online Support
Siemens AG
Filter criteria for entries
All Products
My Products
Product tree
 
 
Clear all filters
Product
Search product
Entry type
 
Date
Task
Thumbnail

6ES7336-4GE00-0AB0
SM 336, f.AI 6 X 0/4 ... 20mA HART
SIMATIC S7, Analog input SM 336, 6 AI; 15 bit; fail-safe analog inputs for SIMATIC Safety, with HART support, up to Category 4 (EN 954-1)/ SIL3 (IEC61508)/PLE (ISO13849), 1x 20-pole

  • Save filter
  • Load filter
  • email on update
16
Entries
Filtered by
'
6ES7336-4GE00-0AB0
'
and
'
FAQ
'
 
Entries per page: 20 50 100
...
1
...
FAQ Information about product-related environmental protection

Validity: Products of the Operating Company DI (Digital Industries) and Business Unit SI CP (Control Products) of Siemens AG.

06/17/2019
ID: 39200038
(19)
FAQ Why does the error message 2988:2074 appear when quitting the window for setting the IO address of a fail-safe ET 200M module in the HW Config?

When setting the IO addresses of a fail-safe ET 200M module it might happen that you get the following error message when quitting the configuration window: Object Properties (2988:2074): "The IO address: [IO initial addresses] must not exceed the maximum process image of the CPU. For the set process image and used module the maximum permissible address is [xxxx]."

03/05/2019
ID: 109763508
(1)
FAQ How do you download the 3D, CAx and ePLAN data for the SIMATIC products?

You can use the CAx download manager to access the latest product data for your CAD or CAE system.

09/20/2018
ID: 89671877
(3)
FAQ How can you combine fail-safe and standard modules in the ET 200 stations?

With ET 200S and ET 200M you can use fail-safe and standard modules combined. Additional measures have to be taken for some modules in this respect.

07/07/2016
ID: 14198063
(6)
FAQ How do you standardize and destandardize analog values with STEP 7 (TIA Portal)?

Contrary to binary signals, analog signals take any number of values within a specific range. You have to convert or standardize and destandardize the analog values before you can process, display or output them.

07/04/2016
ID: 77316903
(16)
FAQ How many ET 200M bus modules can you mount on a deep ET 200M mounting channel?

The number of ET 200M bus modules you can mount on an ET 200M mounting channel depends on the following:

04/13/2016
ID: 109483722
(4)
FAQ How do you operate an ET 200M IM 153-2BAx1/-2BAx2 on a redundant ABB system, the AC800M?

The ABB system does not fully support the standard redundancy in accordance with "Specification Slave Redundancy V1.2, Nov. 2004 by the PROFIBUS User Organization; Order No: 2.212".

04/12/2016
ID: 24220825
(2)
FAQ Why is the F-AI 6ES7336-4GE00-0AB0 rendered passive when HART communication is enabled?

With enabled HART communication the F-AI is rendered passive and the diagnostics buffer displays error message 16#F580:0F01. You can prevent this by parameterizing the "HART gateway".

10/22/2015
ID: 109479604
(4)
FAQ How do you find the UL certificates for SIMATIC modules?

The following instructions show you how to find the UL certificate on our Support pages taking the example of an S7-1500 digital input module (article number: 6ES7 521-1BL00-0AB0).

10/19/2015
ID: 102840331
(3)
FAQ SINAMICS S120, CU310-2 PN, CU320-2 PN: Maintenance request when allocating NameOfStation

Maintenance request when allocating NameOfStation. The MAINT LED of the CPU lights up yellow.

07/22/2015
ID: 109478287
(2)
FAQ Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas

SIMATIC modules of the product families S7-300 S7-400 ET 200M ET 200S ET 200iSP TDC are also approved for implementation in environments with high concentrations of corrosive gas in compliance with ISA–S71.04 severity level G1; G2; G3. ...

03/26/2013
ID: 28569857
(2)
FAQ Which fail-safe signal modules of the distributed I/O can be combined with which fail-safe controllers?

Description There are various fail-safe modules of the distributed I/O available depending on the fail-safe controller used. ...

08/08/2012
ID: 14196393
(4)
FAQ Why are sporadically not all the modules parameterized when starting up a software redundancy configuration with 2 IM 6ES7153-2BA..-....?

Description When implementing a software redundancy configuration with two IM 6ES7153-2BA..-.... (hereinafter call IM), it might happen that when both IMs are switched on at the same time not all the modules (SM3xx, FM3xx, CP3xx, etc., hereinafter called IO) are not parameterized when the IMs are started up. ...

11/26/2010
ID: 46802313
(0)
FAQ How does the analog input of an S7-300 for current measuring (4-20 mA) react when the current flow is less than 4 mA?

Description In the case of underflow of the 4 mA limit, a negative value is output (e.g. -1 is output for 3.9995mA), which becomes steadily smaller until at 1.185 mA the value -4864 (decimal) or ED00 (hexadecimal) is reached. ...

06/07/2010
ID: 9375207
(0)
FAQ Which manuals for ET 200M are available for downloading in A&D Product Support?

Description: The tables below list the documentation concerning the Distributed I/O Device ET 200M. ...

10/30/2006
ID: 24092648
(0)
FAQ Choosing a partial process image depends on the address area in the CPU process image

QUESTION: Why can I not set a partial process image for my I/O module? ANSWER:...

08/22/2003
ID: 14955563