×
Siemens Industry Online Support
Siemens AG
Filter criteria for entries
All Products
My Products
Product tree
 
 
Clear all filters
Product
Search product
Entry type
 
Date
Thumbnail
Complete Package S7-300
Complete Package S7-300
  • Save filter
  • Load filter
  • e-mail on update
20
Entries
Filtered by
'
6ES7398-0AA00-0BA0
'
 
Entries per page: 20 50 100
...
1
...
FAQ How do you find the right successor product if the existing product has already been discontinued?

In the following, you will find instructions on how to replace the discontinued module and determine compatibility information.

12/09/2021
ID: 109804833
(0)
FAQ How are the variables stored in the temporary local data?

In the following we explain the local data addressing with S7-300/S7-400.

07/28/2021
ID: 291495
(1)
FAQ Implementation of SIMATIC modules in environments with high concentrations of corrosive gas

SIMATIC modules of the product families S7-300, S7-400, S7-1500, ET 200M, ET 200S, ET 200SP, ET 200SP HA, ET 200MP, ET 200iSP, TDC are also approved for implementation in environments with high concentrations of corrosive gas in compliance with ISA–S71.04 severity level G1; G2; G3. ...

07/07/2021
ID: 28569857
(3)
FAQ Where can you find the latest updates of the operating systems for the CPUs S7-31x, IM15x and BM147?

Overview of the firmware versions of all S7-300 CPUs

04/28/2021
ID: 26290163
(5)
FAQ Why does the message "16# 4546 STOP caused by CPU memory management” appear in the diagnostics buffer with an S7-300 CPU?

You get this message in the diagnostics buffer of STEP 7 (TIA Portal) if the S7-300 CPU recognizes an access error to the MMC.

10/12/2020
ID: 109782017
(2)
Application example Configuration of a SIPLUS HCS4x00 Heating Control System in STEP 7 V5.5

Library for controlling the SIPLUS HCS4x00 heating control system as PROFINET IO device or as PROFIBUS DP slave on a SIMATIC S7-300/S7-400.

09/28/2018
ID: 109742271
(3)
FAQ Comparison: How are the communication resources managed in the S7-300 and S7-1500?

Management of the communication resources of a SIMATIC depends on the type of controller. With the S7-300 you have to respect a number of details before determining the maximum number of devices you can connect for the configuration. The communication management of the S7-1500 has simpler regulations.

06/12/2017
ID: 109747092
(4)
FAQ In STEP 7 (TIA Portal), how can you input, read out and edit the date and time for the CPU modules?

Description In order to input or read out the date and time of CPU clocks you need the data type "DT" (DATA_AND_TIME) for S7-300/S7-400 and data type "DTL" for S7-1200/S7-1500.

06/29/2016
ID: 43566349
(27)
FAQ How do you install the Software Redundancy V1.2 (SP3) in MS Windows 7 (or higher)?

In MS Windows 7 (or higher) you can only use single components of the Software Redundancy V1.2. It is not possible to install the software completely.

05/09/2016
ID: 109482402
(3)
FAQ In STEP 7 (TIA Portal), how can you count forwards and backwards in a bandwidth between -2147483648 and +2147483647?

You can use the FB "Dcount" from the attached library to count forwards and backwards in the above-mentioned bandwidth.

05/06/2016
ID: 39309294
(1)
FAQ In STEP 7 (TIA Portal), how do you convert the number of days, hours, minutes and seconds into milliseconds?

You can use the function "TimeToMillisec" to determine the number of milliseconds from the number of days, hours, minutes and seconds.

02/23/2016
ID: 43184859
(4)
FAQ Which images, graphics, symbols and screenshots are available for SIMATIC industrial automation systems?

The picture database includes a large number of photos, graphics, 3D models and engineering data in various versions all ready for free downloading.

02/12/2016
ID: 13999030
(7)
FAQ How do you save the setpoint values (actual values) of the SIMATIC S7-300 which are changed online during commissioning?

During commissioning, certain values in the data blocks are changed for the plant. These can be control parameters, limit values, etc. These changes are often made directly in the CPU. In order to retain these changes, the data has to be saved beforehand.

12/03/2015
ID: 109478260
(5)
FAQ Which information is entered in the diagnostic buffer of the SIMATIC S7 CPU with STEP 7 V5.x?

System diagnostics is for recognizing, evaluating and displaying errors that occur in an automation system. For this there is a diagnostic buffer in each CPU and module that supports system diagnostics, in which detailed information on all the diagnostic events is entered.

06/17/2015
ID: 14960968
(7)
Application example ADEPT Robot Control using a SIMATIC S7-300 Controller

Task Robot applications in industry are very frequently integrated into production lines that are controlled by programmable logic controllers. Usually the robot application is a seperate unit acting independently from the production line controller and needs to be supplied with data required for...

09/26/2013
ID: 79100154
(3)
Application example Connection between PROFIBUS Networks and DeviceNet by Anybus X-Gateways

Problem:   The increasing networking of different systems also increases the necessity for SIMATIC products to communicate with devices of third-party suppliers. In this connection, Allen-Bradley or Rockwell products, which have a high market penetration especially in the USA, are of pa...

01/10/2007
ID: 23902276
(0)
Application example Communication between SIMATIC S7 and Allen-Bradley ControlLogix CPUs via Ethernet: Use of "Echochange" gateways

Task:   With the networking of different systems increasing, the necessity of SIMATIC products being able to communicate with devices of external providers also increases. Here, Allen-Bradley or Rockwell products which especially penetrate the US market are of special interest. ...

11/14/2006
ID: 23901499
(2)
Application example Communication between SIMATIC S7-CPUs on PROFIBUS and Allen-Bradley Controllers via SST PROFIBUS Scanner

Problem:   The increasing networking of different systems also increases the necessity for SIMATIC products to communicate with devices of third-party suppliers. In this connection, Allen-Bradley or Rockwell products, which have a high market penetration especially in the USA, are of pa...

11/14/2006
ID: 23809864
(0)
FAQ Memory reset request by the CPU

QUESTION: Why does my S7-300 CPU stop with a request for a memory reset after having transferred a project onto my MMC?  ...

07/30/2003
ID: 16503831
(0)
Product note S7-300 Complete Package with CPU 312IFM + STEP 7 Mini

Concerns products with the Catalog Nos.: 6ES7 398-0AA00-0AA0 S7-300 Complete Package, German 6ES7 398-0AA00-0BA0 S7-300 Complete Package, English ...

For products: 6ES7398-0AA00-0BA0, 6ES7398-0AA00-0AA0
09/19/1996
ID: 4326740
(0)
 
Entries per page: 20 50 100
...
1
...