6GK7443-1EX10-0XE0
COMMUNICATION PROCESSOR CP 443-1
SIMATIC NET, CP 443-1 COMMUNICATIONS PROCESSOR FOR CONNECTION OF SIMATIC S7-400 W. INDUSTR. ETHERNET VIA ISO AND TCP/IP, S7 COMM., FETCH/WRITE, SEND/RECEIVE, WITH AND W/O RFC, 10/100 MBIT

  • Save filter
  • Load filter
  • email on update
121
Entries
Filtered by
'
6GK7443-1EX10-0XE0
'
 
Entries per page: 20 50 100
...
1
2
3
4
5
...
FAQ How do you configure your PC as NTP server?

The Network Time Protocol (NTP) is a standard for synchronizing computer system clocks over package-based communication networks.

04/12/2018
ID: 22144502
(28)
FAQ Which ports are used by the various services for data transfer via TCP and UDP and what should you watch out for when using routers and firewalls?

The various services each use their own port for data transfer via TCP and UDP.

07/05/2017
ID: 8970169
(17)
FAQ What is RFC1006 and what do I need this service for?

RFCs (Request for Comments) are documents in which technical components, like the architecture of the internet, the structure of protocols and the form of e-mail headers, for example, are described in detail.

04/03/2017
ID: 15048962
(2)
Certificate Confirmation, Manufacturer

Chinese Quality Check Mark A0210

10/20/2016
ID: 109742369
(1)
FAQ Which communication services are supported by the Industrial Ethernet CPs of SIMATIC S7-400?

The Industrial Ethernet CPs of SIMATIC S7-400 differ in terms of their hardware interfaces and communication utilities including quantity frameworks.

10/06/2016
ID: 15368142
(6)
FAQ Manual-based information on the topic of "CPU and STEP 7 compatibility"

In an automation system, a communication processor (CP) can only be operated with a CPU. In the system test, the relevant CPUs are tested with the separate Ethernet CPs and released accordingly.

07/20/2016
ID: 26561772
(6)
Manual Security with SIMATIC S7-Controller

03/2016, System manual

03/11/2016
ID: 90885010
(6)
Application example Security with SIMATIC-S7 controllers

This document gives an overview which security mechanisms the automation components have integrated for protecting the system integrity against cyber attacks and unauthorized access by users or non-company persons.

03/11/2016
ID: 77431846
(2)
FAQ How do you use and configure IP multicast for UDP connections in Industrial Ethernet CPs / CMs?

IP multicast is a special connection option that is supported and can be configured only for UDP connections (UDP - User Datagram Protocol) in Industrial Ethernet CPs / CMs. IP multicast was established to send messages from one station to multiple partner stations.

10/16/2015
ID: 9822272
(2)
FAQ SINAMICS S120, CU310-2 PN, CU320-2 PN: Maintenance request when allocating NameOfStation

Maintenance request when allocating NameOfStation. The MAINT LED of the CPU lights up yellow.

07/22/2015
ID: 109478287
(2)
Certificate EMC, Radio Equipment Type Approval Certificate

KCC Registration of Broadcasting and Communication Equipments Korea for SIMATIC NET S7-400CP KCC-REM-S49-S7400CP

06/17/2015
ID: 59535345
(0)
FAQ How do you determine the status of a communications connection, S7 connection, for example, in STEP 7 V5.x?

For the S7-300, S7-400 and PC Station the communications connections like S7 connections are configured in NetPro in STEP 7 V5.x. You can determine the status of the communications connections in NetPro using the function "Activate/Deactivate Connection Status".

06/08/2015
ID: 109476463
(9)
Manual Catalog IK PI - Industrial Communication SIMATIC NET

2015, Catalog, E86060-K6710-A101-B8-7600, E86060-K6710-A101-B8-7600

03/12/2015
ID: 109745642
(0)
FAQ Where can you find information about the SICLOCK system?

Description The SICLOCK system is a system that can be parameterized, and is modular and optimally adjusted for time synchronization of plants of all sizes. ...

01/21/2015
ID: 34676910
(0)
Application example Industrial Communication (Videos)

Introduction Over the past few years, an incredible variety of new products and features have been developed in the field of industrial communication: The aim of the videos you will find in this entry is to make it easier for you to get an overview of the variety of products and to help you bette...

12/10/2014
ID: 22531370
(5)
Application example AS-AS Communication between process control system PCS 7 and Freelance 800F by ABB

Task In the case of an expansion or modernization of large plants it is necessary that various process control systems are linked to be able to exchange important data quickly and easily. Linking different process control systems may be very complex due to a big age difference or different manufa...

10/31/2014
ID: 39168210
(0)
Application example Setting up a secure VPN Connection between SCALANCE S and CP x43-1 Adv. Using a static IP Address.

Task Due to increased networking through Ethernet, remote diagnostics and/or remote maintenance are of great importance in modern automation systems. Today's Internet access mechanisms (wireless, broadband) and the security components from Siemens are an ideal combination for industrial remote co...

10/21/2014
ID: 99681025
(0)
Application example Programming an OPC UA .NET Client with C# for the SIMATIC NET OPC UA Server

Problem   To realize a data link between a controller and a PC system, standardized mechanisms are preferably used to ensure that such a data exchange remains independent of the used bus system or protocol or even manufacturer. OPC UA combines this functionality and additionally offers ...

09/04/2014
ID: 42014088
(6)
Certificate General Product Approval, UL, UL

UL-Listing USA: "Programmable Controllers" UL-File: NRAG.E85972

05/12/2014
ID: 20710588
(0)
FAQ How do you check a TCP or UDP connection if there is no communication partner?

Instructions If you want to test an application with the TCP or UDP communication type but there is no partner station, you can use a PC for the test. No additional software is required for this on the PC. Proceed as follows. In the settings of the TCP/UDP connection you set the IP of the partner to the IP address of the PC. Enter number 7 or 9 as the partner port (see below for difference). Load the configuration. Test the connection and check the conne ...

04/02/2014
ID: 90528095
(2)
 
Entries per page: 20 50 100
...
1
2
3
4
5
...