×
Siemens Industry Online Support
Siemens AG
Filter criteria for entries
All Products
My Products
Product tree
 
 
Clear all filters
Product
Search product
Entry type
 
Date
Task
  • Save filter
  • Load filter
  • email on update
12873
Entries
Filtered by
'
FAQ
'
 
Entries per page: 20 50 100
...
1
2
3
4
5
...
FAQ Settings of the ports for secure VPN connections with SINEMA Remote Connect

To enable a secured VPN connection you have to set up a port release on the VPN client side (connection to the internet) and port forwarding on the VPN server side (ports used in the server).

06/14/2019
ID: 109745584
FAQ SINUMERIK 828D X130 Remote access via VNC Viewer

With the 828D as of software version >=V4.8 SP4, it is mandatory to assign a VNC password.

For products: 6FC53..
06/14/2019
ID: 109767953
FAQ SINAMICS V90 PN: Re-powering on V90 PN with firmware V1.02 or higher can cause communication disconnection between V90 and PLC

Despite the correct setting, communication with the PLC may remain disconnected after a V90 PN is re-powered.

06/14/2019
ID: 109768408
FAQ What should you watch out for with the "Save as..." option with PCS 7 multiprojects with Logic Matrix?

When using the "Save as..." option with PCS 7 multiprojects with Logic Matrices you must pay attention to a number of things to ensure proper saving of the project.

06/12/2019
ID: 109767445
FAQ How do you create your own certificates for panels?

Data security when transferring via the internet must be ensured for the remote control of HMI operator panels via Sm@rtClient. Client and server certificates are installed for this. The FAQ response describes how to create self-signed certificates and where these are stored on the PC and operator panel.

06/12/2019
ID: 109763500
FAQ Which hardware and functions of SINAMICS G130, G150, S120, S150 and SINAMICS MV are supported by SINAMICS Startdrive V15 and V15.1?

Overview of the supported hardware and functions of SINAMICS drives based on the CU320-2 by SINAMICS Startdrive V15 and V15.1

06/11/2019
ID: 109761180
FAQ Which WinCC/WebNavigator client can be connected to which WinCC/WebNavigator server?

Generally each WinCC/WebNavigator client can be connected with each WinCC/WebNavigator server of the same or older version. This information is valid for versions V7.0 to V7.5.

06/05/2019
ID: 17204272
FAQ Which Microsoft Updates have been tested for compatibility with SIMATIC PCS 7?

Microsoft regularly rectifies security gaps in its products and makes these fixes available to users via product updates.

06/05/2019
ID: 18490004
FAQ Why do you have to log in and register for downloading export-restricted software and what data do you need for this?

Information about software packages or components that are subject to national and European export regulations and US re-export regulations.

06/05/2019
ID: 109744535
FAQ Room thermostats RDG160T Version F: Parameter access handling

Affected are all RDG160T Serie F, production date 28 February 2019 to May 2019.

For products: S55770-T343
06/05/2019
ID: 109768144
FAQ Which EPLAN data is required for AML data exchange with STEP 7 (TIA Portal)?

The settings in the EPLAN macros described in this entry are required for AML data exchange between the TIA Selection Tool, EPLAN and STEP 7 (TIA Portal).

06/04/2019
ID: 109766653
FAQ How do you connect the Energy Manager to Desigo CC with OPC UA?

The Desigo CC software forwards the data via OPC DA. The Energy Manger has an OPC UA client. The OPC DA/UA wrapper establishes the connection.

06/04/2019
ID: 109765039
FAQ How do you manage license keys stored on the server and operate the Automation License Manager as license server for VMware Workstation?

You can use license keys located on a central computer (server) on a local computer and operate the ALM as license server for VMware Workstation.

06/04/2019
ID: 18602618
FAQ 3RW.. Soft Starter: Is it possible to feed backwards?

This article contains a statement on the connection of the voltage.

06/04/2019
ID: 23680902
FAQ How do you work with the Siemens EPLAN Macros ET 200SP?

The attached PDF document gives you detailed information.

06/04/2019
ID: 109766667
FAQ SINUMERIK: Which ports are open in the different software versions on the X130?

In the Basesys.ini there is the item "FirewallOpenPorts". Which ports are open when there are not entries here?

06/04/2019
ID: 109767356
FAQ How do you import signals, parameters, Control Modules and Hardware into the Plant Automation Accelerator (PAA) with Excel Import?

You can use Excel Import to import the following data into the PAA: signals, parameters, Control Modules (CM) and hardware

06/04/2019
ID: 109761468
 
Entries per page: 20 50 100
...
1
2
3
4
5
...