- Save filter
- Load filter
- e-mail on update
The new Layer 2 product line SCALANCE XCM-300 expands the well-known SCALANCE portfolio and will include a wide variety of product versions in the future. The first product is the SCALANCE XCM332 with 32 ports. The SCALANCE XCM332 is hereby released for sale and delivery with restrictions. In the restricted release, the devices have CE, EAC and RCM certification.
Urgent update required. AT&T will begin sunset of their 3G network in February 2022. After this time, RUGGEDCOM devices with 3G/4G fallback feature will no longer work on AT&T’s network.
The SCALANCE XC-200 product line is being expanded to include PoE versions.
Siemens has expanded its portfolio with the RUGGEDCOM RPS2410 600W power supply. The product is now available for ordering
Firmware version V4.3.1 is now being made available for the SCALANCE XB-200, XC-200, XP-200, XF-200BA,XF-200BA DNA and XR-300WG as a download.
Beginning October 1st, 2022, the following orderable options and line modules for RUGGEDCOM products will be declared discontinued due to lack of demand and in order to optimize the overall portfolio.
Firmware version V4.3.1 is announced for the beginning of 11/2021 for the SCALANCE XB-200, XC-200, XP-200, XF-200BA, XF-200BA DNA and XR-300WG.
The proven SIMATIC ET 200SP HA, (Scalable Peripheral System, High Availability) offers you the optimal basis for the digital challenges in the process industry.
CloudConnect v1.2 running on the RUGGEDCOM RX1400, or the RUGGEDCOM APE1808 is released for delivery. CloudConnect hosted on the RX1400, or the APE1808, provides an all-in-one solution for secure IIoT device to cloud connectivity in harsh environments.
Announcement of product phase-out LOGO! CSM 230 (6GK7177-1FA10-0AA0)
The SCALANCE X-200 firmware update version 5.2.5 can now be downloaded for free from Product Support.
The SCALANCE X-200IRT firmware update version 5.5.1 can now be downloaded free of charge from Product Support
Sales and delivery release SCALANCE XR326-2C PoE WG, XR108-2PoE WG, PSR9230PoE
The SCALANCE X-200IRT firmware update version 5.5.0 can now be downloaded free of charge from Product Support.
If Loop Detection is enabled and the switch is restarted, the switch may no longer be accessible via its configuration and diagnostics interfaces in certain configurations.