×
Siemens Industry Online Support
Siemens AG
Filter criteria for entries
All Products
My Products
Product tree
 
 
Clear all filters
Product
Search product
Entry type
 
Date
Task
  • Save filter
  • Load filter
  • email on update
773
Entries
Filtered by
'
Converters
'
and
'
FAQ
'
 
Entries per page: 20 50 100
...
1
2
3
4
5
...
FAQ Compatibility Tool for Automation and Drive Technology

The Compatibility Tool is a function provided by the Industry Online Support with which you can select compatible software products or check the compatibility of existing configurations.

09/03/2019
ID: 64847781
(123)
FAQ SINAMICS S120 in Startdrive: Upload aborted because of an inconsistency in the component numbers in drive objects

The upload in Startdrive is not possible if there is a component number inconsistency in the drive objects. This FAQ response gives you a remedy for this.

For products: 6SL3040-1MA01-0AA0, 6SL3040-1MA00-0AA0
08/30/2019
ID: 109770000
(2)
FAQ Which firmware version is required for SINAMICS S120 Chassis-2 devices?

The SINAMICS S120 Chassis-2 product family must be operated with a FW 5.2 HF1 or higher. An operation with FW less than 5.2 HF1 is not permitted.

08/26/2019
ID: 109768875
(0)
FAQ Startdrive V15.1: Upload of a drive unit SINAMICS S120 with deleted second axis of a Double Motor Module

If you create a Double Motor Module with only one axis in a STARTER project, an error-free upload in Startdrive is not possible.

08/26/2019
ID: 109769533
(1)
FAQ Restriction on enabling UMAC (User Management and Access Control) protection in Startdrive V15.1 and V15.1 UPD1

When you enable UMAC protection in a project with Startdrive V15.1 or V15.1 UPD1 and SINAMICS G drives in a group folder, the project becomes unusable.

08/08/2019
ID: 109769004
(1)
FAQ Startdrive V15.1 and SINAMICS S120: Abort of upload and export/import of SINAMICS S120 in STARTER when configuring asynchronous motors with manual data input in Startdrive

If a project configured with Startdrive V15.1 with SINAMICS S120 and motor modules with asynchronous motors with manual data input are loaded into SINAMICS S120, an upload of the device to the project is aborted with STARTER.

07/08/2019
ID: 109767402
(0)
FAQ How to mount the gate-cathode wires between TAS-card and thyristor at an air-cooled SINAMICS GL150 / SL150?

Advice to mount the gate-cathode-wires between TAS-card and thyristor at an air-cooled SINAMICS GL150 / SL150

For products: 6SL385., 6SL386.........., 6SL3850.........
06/25/2019
ID: 109768652
(0)
FAQ Information about product-related environmental protection

Validity: Products of the Operating Company DI (Digital Industries) and Business Unit SI CP (Control Products) of Siemens AG.

06/17/2019
ID: 39200038
(18)
FAQ SINAMICS V90 PN: Re-powering on V90 PN with firmware V1.02 or higher can cause communication disconnection between V90 and PLC

Despite the correct setting, communication with the PLC may remain disconnected after a V90 PN is re-powered.

06/14/2019
ID: 109768408
(1)
FAQ Which hardware and functions of SINAMICS G130, G150, S120, S150 and SINAMICS MV are supported by SINAMICS Startdrive V15 and V15.1?

Overview of the supported hardware and functions of SINAMICS drives based on the CU320-2 by SINAMICS Startdrive V15 and V15.1

06/11/2019
ID: 109761180
(6)
FAQ SINAMICS V20: How to correctly connect cables to V20 I/O terminals ?

05/31/2019
ID: 109766619
(0)
FAQ What advantages does the Smart Access Module offer customers in conjunction with a SINAMICS V20 frequency converter?

The Smart Access Module for the SINAMICS V20 is a web server module that allows the operator quick and easy access to the converter.

05/29/2019
ID: 109767666
(1)
FAQ SINUMERIK: The extension of SINAMICS S120 Combi with a SINAMICS Capacitor Module does not work

The extension of SINAMICS S120 Combi with a SINAMICS Capacitor Module (6SL3100-1CE14-0AAX) is not possible, SINAMICS S120 Booksize modules must be used.

05/24/2019
ID: 109767628
(3)
FAQ Why does my SINAMICS S210 3AC200-480V converter show warning A30016 even though the mains voltage is present?

The reason for the warning A30016 may be an incorrect connection to terminal X4 (braking resistor).

05/23/2019
ID: 109767864
(0)
FAQ SIMATIC S7: What is the meaning of the following event IDs: "16# 08:9000" to "16# 08:9013"?

The event IDs "16# 08:9000" to "16# 08:9013" indicate faults and warnings for a drive.

05/23/2019
ID: 109764509
(1)
FAQ SINAMICS V20: Why I get fault F23?

Cloning a drive with firmware before 3.9.5 to a drive with firmware 3.9.5 may cause F23 to occur.

05/16/2019
ID: 109766987
(0)
FAQ SINAMICS G120: Which screws have to be used to mount a IOP-2 or BOP-2 into the door of a cabinet?

Please check which version of the Operators Panel you have and select the correct screws before installing the door mounting kit.

05/15/2019
ID: 109766997
(0)
FAQ SINAMICS G120: How to change message type, response and acknowledge mode of a fault

This FAQ describes how to change message type, response and acknowledge mode of a fault.

05/08/2019
ID: 109767372
(1)
FAQ SINAMICS G120: Automatic restart after main power failure but with external 24V supply still on

This FAQ shows the way to implement automatic restart after main power failure but with external 24V supply still on.

05/08/2019
ID: 109767371
(0)
FAQ SINAMICS G120: Why can’t the value of p1800 (pulse frequency setpoint) be modified?

There are restrictions to change p1800 (pulse frequency setpoint). Modification of p1800 has something to do with p1910 (motor data identification selection) in SINAMICS G120.

05/06/2019
ID: 109767398
(0)
 
Entries per page: 20 50 100
...
1
2
3
4
5