×
Siemens Industry Online Support
Siemens AG
Filter criteria for entries
All Products
My Products
Product tree
 
 
Clear all filters
Product
Search product
Entry type
 
Date
Task
  • Save filter
  • Load filter
  • email on update
666
Entries
Filtered by
'
Low voltage converters
'
and
'
FAQ
'
 
Entries per page: 20 50 100
...
1
2
3
4
5
...
FAQ How do you do a fail-safe switch-off of standard modules?

You can do a fail-safe switch-off of various SIMATIC standard modules. This entry shows which modules apply here.

11/08/2019
ID: 39198632
(19)
FAQ Why I get a message when I open my TIA Portal project, after updating the HSP 0185 (SINAMICS V90 PN) for TIA Portal V15.1 from V1.0 to V2.0

The HSP 0185 V2.0 hosts 6SL3210-5FB10-1UF2 and 6SL3210-5FB10-2UF2 but not 6SL3210-5FB10-1UF1 and 6SL3210-5FB10-2UF1 any more.

For products: 6SL3210-5FB10-1UF1, 6SL3210-5FB10-2UF1
10/30/2019
ID: 109772163
(0)
FAQ Overview of the engineering functions supported in Startdrive V15.1 with SINAMICS DCC V15.1

Overview of the engineering functions of SINAMICS DCC V15.1

10/30/2019
ID: 109772314
(0)
FAQ How to obtain and install the G120X PROFINET GSDML or PROFIBUS GSD file directly from the G120X Control Unit into a TIA Portal project

Startdrive does not support SINAMICS G120X. If you want to establish a PROFINET or PROFIBUS network connection to a G120X, or add it to an existing configuration, you have to use a GSDML or GSD file.

For products: 6SL3220.
10/28/2019
ID: 109772109
(0)
FAQ Clarification for the use of STO with SINAMICS G120X and PM240-2 for large installation heights

When operating STO with SINAMICS G120X or PM240-2 at high installation altitudes certain criteria must be observed.

10/07/2019
ID: 109772041
(1)
FAQ G110M Braking Resistor ratings Internal and External

Minimum Braking resistor values should be adhered to, to prevent damage to the inverter.

For products: 6SL3501-0BE18-8AA0, 6SL3501-0BE22-0AA0
09/25/2019
ID: 109771766
(1)
FAQ ATEX application with SINAMICS inverter

For ATEX applications, a topology consisting of a SINAMICS G120/G120C inverter, SIRIUS 3RN2 thermistor motor protection relay and an explosion-proof motor is described here.

09/25/2019
ID: 109771821
(0)
FAQ Which firmware version is required for SINAMICS S120 Chassis-2 devices?

The SINAMICS S120 Chassis-2 product family must be operated with a FW 5.2 HF4 or higher. An operation with FW less than 5.2 HF4 is not permitted.

09/18/2019
ID: 109768875
(0)
FAQ Compatibility Tool for Automation and Drive Technology

The Compatibility Tool is a function provided by the Industry Online Support with which you can select compatible software products or check the compatibility of existing configurations.

09/03/2019
ID: 64847781
(128)
FAQ SINAMICS S120 in Startdrive: Upload aborted because of an inconsistency in the component numbers in drive objects

The upload in Startdrive is not possible if there is a component number inconsistency in the drive objects. This FAQ response gives you a remedy for this.

For products: 6SL3040-1MA01-0AA0, 6SL3040-1MA00-0AA0
08/30/2019
ID: 109770000
(2)
FAQ Startdrive V15.1: Upload of a drive unit SINAMICS S120 with deleted second axis of a Double Motor Module

If you create a Double Motor Module with only one axis in a STARTER project, an error-free upload in Startdrive is not possible.

08/26/2019
ID: 109769533
(2)
FAQ Restriction on enabling UMAC (User Management and Access Control) protection in Startdrive V15.1 and V15.1 UPD1

When you enable UMAC protection in a project with Startdrive V15.1 or V15.1 UPD1 and SINAMICS G drives in a group folder, the project becomes unusable.

08/08/2019
ID: 109769004
(1)
FAQ Startdrive V15.1 and SINAMICS S120: Abort of upload and export/import of SINAMICS S120 in STARTER when configuring asynchronous motors with manual data input in Startdrive

If a project configured with Startdrive V15.1 with SINAMICS S120 and motor modules with asynchronous motors with manual data input are loaded into SINAMICS S120, an upload of the device to the project is aborted with STARTER.

07/08/2019
ID: 109767402
(0)
FAQ Information about product-related environmental protection

Validity: Products of the Operating Company DI (Digital Industries) and Business Unit SI CP (Control Products) of Siemens AG.

06/17/2019
ID: 39200038
(19)
FAQ SINAMICS V90 PN: Re-powering on V90 PN with firmware V1.02 or higher can cause communication disconnection between V90 and PLC

Despite the correct setting, communication with the PLC may remain disconnected after a V90 PN is re-powered.

06/14/2019
ID: 109768408
(1)
FAQ Which hardware and functions of SINAMICS G130, G150, S120, S150 and SINAMICS MV are supported by SINAMICS Startdrive V15 and V15.1?

Overview of the supported hardware and functions of SINAMICS drives based on the CU320-2 by SINAMICS Startdrive V15 and V15.1

06/11/2019
ID: 109761180
(6)
FAQ SINAMICS V20: How to correctly connect cables to V20 I/O terminals ?

05/31/2019
ID: 109766619
(0)
FAQ What advantages does the Smart Access Module offer customers in conjunction with a SINAMICS V20 frequency converter?

The Smart Access Module for the SINAMICS V20 is a web server module that allows the operator quick and easy access to the converter.

05/29/2019
ID: 109767666
(1)
FAQ SINUMERIK: The extension of SINAMICS S120 Combi with a SINAMICS Capacitor Module does not work

The extension of SINAMICS S120 Combi with a SINAMICS Capacitor Module (6SL3100-1CE14-0AAX) is not possible, SINAMICS S120 Booksize modules must be used.

05/24/2019
ID: 109767628
(3)
FAQ SIMATIC S7: What is the meaning of the following event IDs: "16# 08:9000" to "16# 08:9013"?

The event IDs "16# 08:9000" to "16# 08:9013" indicate faults and warnings for a drive.

05/23/2019
ID: 109764509
(1)
 
Entries per page: 20 50 100
...
1
2
3
4
5