×
Siemens Industry Online Support
Siemens AG
Filter criteria for entries
All Products
My Products
Product tree
 
 
Clear all filters
Product
Search product
Entry type
 
Date
  • Save filter
  • Load filter
  • e-mail on update
41
Entries
Filtered by
'
Fault-tolerant CPUs
'
and
'
Product note
'
 
Entries per page: 20 50 100
...
1
2
3
...
Product note Delivery Release for S7-400H V6 Including PROFINET Support

  The new S7-400H controllers including PROFINET support are herewith released for delivery. ...

04/09/2020
ID: 59903098
(7)
Product note End of the SIMATIC S5 product life cycle

For the SIMATIC S5 system, the product life cycle ends on 30 September 2020. As of 1 October 2020, spare parts will not be available and repairs will not be possible. Until 30 September 2020, spare parts can be obtained subject to availability and possibly only in exchange.

02/26/2020
ID: 109776026
(7)
Product note AS Configurator - Parts List

The following is a list of technical specifications and EU declarations of conformity for the individual components of AS bundles.

03/28/2019
ID: 109765448
(4)
Product note Important information on SIMATIC S7-400H safety programs during uninterrupted operation

If a safety program is used (SIMATIC S7 F system), an unscheduled stop may occur after more than 9 years of uninterrupted operation without resetting the CPU. The safety application is transferred into the defined safe state, in stand-alone or solo operation. If the CPUs are used redundantly, the system initially only switches to solo mode.

12/21/2018
ID: 109762993
(3)
Product note SITRAIN Training courses for SIMATIC S7-300/-400

SITRAIN offers a comprehensive training portfolio for know-how communication centered around the topic of SIMATIC S7-300/S7-400.

05/02/2018
ID: 53814828
(1)
Product note Delivery release for SIMATIC S7 F ConfigurationPack V5.5 SP13

The delivery release for SIMATIC S7 F ConfigurationPack V5.5 SP13 is now available for download.

08/10/2017
ID: 109749364
(3)
Product note Delivery release SIMATIC S7 Distributed Safety V5.4 SP5 Update 2

Delivery release for SIMATIC S7 Distributed Safety V5.4 SP5 Update 2. The Safety Option Package update supports Microsoft Windows 10.

08/10/2017
ID: 109749290
(5)
Product note Simultaneous use of the latest CPU firmware V6.0.6 and PROFINET

Please note the following when using the currently recommended firmware version 6.0.6 for the SIMATIC S7-400H CPUs (6ES7412-5HK06-0AB0, 6ES7414-5HM06-0AB0, 6ES7416-5HS06-0AB0, 6ES7417-5HT06-0AB0) simultaneously with PROFINET devices in a fault-tolerant automation system:

02/13/2017
ID: 109745029
(2)
Product note S7-400 CPUs: Undesired behavior with SFC49 "LGC_GADR"

When accessing the diagnostic address of the PROFINET IO system via SFC49 "LGC_GADR", the SIMATIC S7-400 CPU may show an undesired behavior. This does not affect users of the SIMATIC PCS 7 libraries, as these libraries use the diagnostic address of the interface instead of the diagnostic address of the PROFINET IO system.

04/28/2016
ID: 109736598
(1)
Product note S7-400 sync modules and fiber-optic sync cables

Overview of sync modules and fiber-optic sync cables for the SIMATIC S7-400 redundant automation system (H/FH systems)

11/02/2015
ID: 109480288
(3)
Product note New PROFIBUS interface module for ET 200M, PA Link and Y-Link

In connection with SIMATIC PCS 7 systems, starting at the end of May, the PROFIBUS interface module IM 153, article numbers 6ES7153-2BA82-0XB0 and 6ES7153-2BA02-0XB0, will be substituted with successor modules (article numbers 6ES7153-2BA70-0XB0 and 6ES7153-2BA10-0XB0).

05/22/2015
ID: 109475772
(2)
Product note Acknowledgement of alarms in parallel with "Disable" and "Enable" of alarms (when using specific SIMATIC S7-400 CPUs)

When using specific S7-400 CPUs it can happen in very rare cases/configurations that under certain limiting conditions no new alarms are displayed on the control station anymore. ...

06/16/2014
ID: 94682568
(0)
Product note Operation of switched I/Os under Profinet

Under certain limiting conditions a double-sided defect can occur with the H-CPUs V6.0.3.   Please read the additional information below....

03/20/2014
ID: 90039870
(3)
Product note S7 F ConfigurationPack V5.5 SP11 Released for Download

The S7 F ConfigurationPack V5.5 SP11 is herewith released for download. ...

12/20/2013
ID: 85175144
(1)
Product note Updated Product Information following the inclusion of the EC-Declaration of Conformity for failsafe SIMATIC products

Updated Product Information following the inclusion of the EC-Declaration of Conformity in compliance with the EC Machinery Directive 2006/42 EC for failsafe SIMATIC products. ...

01/10/2013
ID: 66996258
(0)
Product note Product Information S7-400H: Firmware Updating in RUN Mode from V4.5.1 to V4.5.2

Potential problem in conjunction with firmware updating in RUN mode with H CPUs from version V4.5.1 to V4.5.2. ...

01/07/2010
ID: 40240573
(0)
Product note Variables Monitoring with H CPUs V4.5.0

Problems have been detected when monitoring variables with H CPUs V4.5.0. Details are described below....

11/24/2008
ID: 32619422
(1)
Product note Forcing with H CPUs V4.5.0

Problems have arisen with the forcing function of H CPUs V4.5.0. See description below....

03/13/2008
ID: 28662081
(0)
Product note S7-400H V4.5 and CPU 412-3H Released for Delivery

The new CPU 412-3H and the innovated CPUs 414-4H and 417-4H are herewith released for delivery. The new CPU 412-3H rounds off the existing spectrum of H CPUs at the lower end, with respect to performance and quantity framework. The innovated CPUs 414-4H and 417-4H now have a larger work memory an...

10/08/2007
ID: 26609412
(1)
Product note New PROFIBUS Interface Modules for ET 200M, DP/PA Link and Y Link for SIMATIC PCS 7

The PROFIBUS interface modules IM 157 for DP/PA Link and Y Link, and IM 153-2 High Feature for ET 200M will be replaced by the spare part compatible IM 153-2 High Feature follow-up module. In addition to the above individual products, this replacement also affects the combination products Y Link,...

06/20/2006
ID: 23372259
(1)
 
Entries per page: 20 50 100
...
1
2
3
...