×
Siemens Industry Online Support
Siemens AG
Filter criteria for entries
Product tree
 
 
Clear all filters
Product
Search product
Entry type
 
Date
Task
  • Save filter
  • Load filter
  • email on update
9
Entries
Filtered by
'
Communications modules
'
and
'
FAQ
'
 
Entries per page: 20 50 100
...
1
...
FAQ What should you watch out for when operating the CPU555 with CP53M0 with regard to the product release of CP53M0 being used?

The CP53M0 must have at least product release 9 when you use it in conjunction with a CPU555.

For products: 6DD1660-0BJ0, 6DD1600-0BB0
06/22/2016
ID: 109738040
FAQ How do you run diagnostics on the PROFIBUS of a CP50M1?

Unwanted reactions might occur when running the diagnostics of PROFIBUS slaves in the SIMATIC Manager. Therefore you should use the FBs DPDIAG and SPSLDG to run the diagnostics.

For products: 6DD1661-0AD1
03/13/2015
ID: 109474577
FAQ Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas

SIMATIC modules of the product families S7-300 S7-400 ET 200M ET 200S ET 200iSP TDC are also approved for implementation in environments with high concentrations of corrosive gas in compliance with ISA–S71.04 severity level G1; G2; G3. ...

03/26/2013
ID: 28569857
FAQ How can you clear communication error 69A1 with an EXM448, EXM448-1 or CP50M0 as slave on the PROFIBUS?

Description of error: In a DP connection between a DP master (for example, PC with CP5613-A2 ) and an EXM448 or an EXM448-1 or a CP50M0 ...

11/17/2008
ID: 24786106
FAQ How do you read and write drive parameters via PROFIBUS DP with the SIMATIC TDC?

Instructions: In order to be able to read and write drive parameters from and to a SIMATIC TDC configuration, you require an extensive configuration of approx. 30 standard CFC function blocks. Pay attention here to the correct interconnection and correct choice of order of processing. ...

For products: 6DD1661-0AD0
01/07/2008
ID: 27206321
FAQ How can the SIMATIC TDC module CP50M1 be configured as a PROFIBUS DP slave?

Instructions: In the following is a description of the configuration steps required for the SIMATIC TDC module CP50M1. In this example 2 bytes are sent and received. ...

For products: 6DD1661-0AD1
10/29/2007
ID: 26699444
FAQ How can the SIMATIC TDC module CP50M1 as DP master read the input data of a DP slave that has been configured by another DP master (direct data exchange - DX)?

Instructions: In the following is a description of the configuration steps required for the SIMATIC TDC module CP50M1. In this example the slave sends and receives 4 bytes to/from its master and send 4 bytes to another master. ...

For products: 6DD1661-0AD1
10/29/2007
ID: 26697791
FAQ What conditions must be fulfilled with the CP50M1 compared with the old CP50M0?

Configuration Notes: Compared with the old CP50M0, it is no longer possible with the CP50M1 to read all the slaves. With the CP50M1 only those slaves can be read which support the function 'Direct Data Exchange'. You can see which of the slaves does this from the Hardware Configuration. ...

For products: 6DD1661-0AD1
07/17/2007
ID: 26026818
FAQ DP/DP coupler with SIMATIC TDC

QUESTION:   How can I use a DP/DP bus coupler with the SIMATIC TDC module CP50 M0 if the CP50 M0 is the bus master? ...

For products: 6DD1661-0AD0, 6DD1600-0BA1
10/05/2004
ID: 19548417